<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: Can‘t find a source file 'PCLIB_CtrlPI_F16_Asm.c' ( MC56F82748 Codewarrior debug find )</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-t-find-a-source-file-PCLIB-CtrlPI-F16-Asm-c-MC56F82748/m-p/1192931#M2026</link>
    <description>&lt;P&gt;Hi, Zhang,&lt;/P&gt;
&lt;P&gt;In order to protect NXP IP, now for the RTCESL package, we only provide the library instead of source code.&lt;/P&gt;
&lt;P&gt;The *.h files include the api function prototype so that you can know the function format.&lt;/P&gt;
&lt;P&gt;sorry for not helping you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
    <pubDate>Thu, 03 Dec 2020 07:15:39 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-12-03T07:15:39Z</dc:date>
    <item>
      <title>Can‘t find a source file 'PCLIB_CtrlPI_F16_Asm.c' ( MC56F82748 Codewarrior debug find )</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-t-find-a-source-file-PCLIB-CtrlPI-F16-Asm-c-MC56F82748/m-p/1192803#M2025</link>
      <description>&lt;P&gt;Add FSLESL in MC56F82748 project .&lt;/P&gt;&lt;P&gt;Can't find a source file 'PCLIB_CtrlPI_F16_Asm.c' (FSLESL only has PCLIB_CtrlPI_F16_Asm.h).&lt;/P&gt;&lt;P&gt;What should I do to&amp;nbsp;find a source file 'PCLIB_CtrlPI_F16_Asm.c' ？&lt;/P&gt;&lt;P&gt;&amp;nbsp;The picture:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="143742f9ltkgbhhlzekgln.png" style="width: 596px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/131612i4CD94307B52A6F76/image-size/large?v=v2&amp;amp;px=999" role="button" title="143742f9ltkgbhhlzekgln.png" alt="143742f9ltkgbhhlzekgln.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 03:30:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-t-find-a-source-file-PCLIB-CtrlPI-F16-Asm-c-MC56F82748/m-p/1192803#M2025</guid>
      <dc:creator>547351265</dc:creator>
      <dc:date>2020-12-03T03:30:51Z</dc:date>
    </item>
    <item>
      <title>Re: Can‘t find a source file 'PCLIB_CtrlPI_F16_Asm.c' ( MC56F82748 Codewarrior debug find )</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-t-find-a-source-file-PCLIB-CtrlPI-F16-Asm-c-MC56F82748/m-p/1192931#M2026</link>
      <description>&lt;P&gt;Hi, Zhang,&lt;/P&gt;
&lt;P&gt;In order to protect NXP IP, now for the RTCESL package, we only provide the library instead of source code.&lt;/P&gt;
&lt;P&gt;The *.h files include the api function prototype so that you can know the function format.&lt;/P&gt;
&lt;P&gt;sorry for not helping you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Thu, 03 Dec 2020 07:15:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Can-t-find-a-source-file-PCLIB-CtrlPI-F16-Asm-c-MC56F82748/m-p/1192931#M2026</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-12-03T07:15:39Z</dc:date>
    </item>
  </channel>
</rss>