<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックError &amp;quot;CCS: Core not responding&amp;quot; via USB TAP (MC56F8135)</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Error-quot-CCS-Core-not-responding-quot-via-USB-TAP-MC56F8135/m-p/1167391#M1976</link>
    <description>&lt;P&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I created a Bareboard Project for MC56F8135, connection: Freescale USB TAP, language: C++. If I tried debug a template program I got:&lt;BR /&gt;"Failed to resume target process.&lt;BR /&gt;CCSProtocolPlugin : CCS: Core not responding" (diagnostic Info is attached)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I tried to flash compiled elf file with "Freescale DSC Flasher". It gave me an error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Performing PROGRAM operation on MC56F8135 through the UTAP . . .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;expected integer but got "{}""&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But if Erasure Mode "Mass Erase", Operation "Erase" is chosen I get&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Performing ERASE operation on MC56F8135 through the UTAP . . .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mass Erasing Target Device . . .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mass Erase Complete"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you help with this problem? I cannot find a solution. Maybe I should check some project settings or check CSS server, or something else?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I use:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;OS: win7 x64 (and I tried win10 x64).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CodeWarrior 11.1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Freescale DSC Flasher 1.2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Connection Server (CSS) v 4.13&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LibUSB v0.1.12.1&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 14 Oct 2020 10:37:49 GMT</pubDate>
    <dc:creator>xcemaxx</dc:creator>
    <dc:date>2020-10-14T10:37:49Z</dc:date>
    <item>
      <title>Error "CCS: Core not responding" via USB TAP (MC56F8135)</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Error-quot-CCS-Core-not-responding-quot-via-USB-TAP-MC56F8135/m-p/1167391#M1976</link>
      <description>&lt;P&gt;&lt;SPAN&gt;Hi.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I created a Bareboard Project for MC56F8135, connection: Freescale USB TAP, language: C++. If I tried debug a template program I got:&lt;BR /&gt;"Failed to resume target process.&lt;BR /&gt;CCSProtocolPlugin : CCS: Core not responding" (diagnostic Info is attached)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I tried to flash compiled elf file with "Freescale DSC Flasher". It gave me an error:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Performing PROGRAM operation on MC56F8135 through the UTAP . . .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;expected integer but got "{}""&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;But if Erasure Mode "Mass Erase", Operation "Erase" is chosen I get&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;"Performing ERASE operation on MC56F8135 through the UTAP . . .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mass Erasing Target Device . . .&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Mass Erase Complete"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Can you help with this problem? I cannot find a solution. Maybe I should check some project settings or check CSS server, or something else?&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I use:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;OS: win7 x64 (and I tried win10 x64).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;CodeWarrior 11.1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Freescale DSC Flasher 1.2&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Connection Server (CSS) v 4.13&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;LibUSB v0.1.12.1&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2020 10:37:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Error-quot-CCS-Core-not-responding-quot-via-USB-TAP-MC56F8135/m-p/1167391#M1976</guid>
      <dc:creator>xcemaxx</dc:creator>
      <dc:date>2020-10-14T10:37:49Z</dc:date>
    </item>
    <item>
      <title>Re: Error "CCS: Core not responding" via USB TAP (MC56F8135)</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Error-quot-CCS-Core-not-responding-quot-via-USB-TAP-MC56F8135/m-p/1173581#M1981</link>
      <description>&lt;P&gt;Hi, Cema&lt;/P&gt;
&lt;P&gt;As you know that the MC56F8135 is end of life, previously, it was not a mainstream product, it is a abridged version of MC56F83xx, that is why the CW tools does not have the initialization file.&lt;/P&gt;
&lt;P&gt;Can you use the latest DSC family for example MC56F83xxx, it's tools is CW for mcu ver11.1, this is the link of MC56F83xxx.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digital-signal-controllers:Digital-Signal-Controllers" target="_blank"&gt;https://www.nxp.com/products/processors-and-microcontrollers/additional-mpu-mcus-architectures/digital-signal-controllers:Digital-Signal-Controllers&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 27 Oct 2020 06:05:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Error-quot-CCS-Core-not-responding-quot-via-USB-TAP-MC56F8135/m-p/1173581#M1981</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-10-27T06:05:12Z</dc:date>
    </item>
  </channel>
</rss>