<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TDA5051A DC Power Line Communication  in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TDA5051A-DC-Power-Line-Communication/m-p/980404#M1758</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the TDA5051A on a 12VDC power line using the schematic below. 7.372MHz independant oscillator, 115.2kHz carrier frequency. I've tried both 600 and 1200 baud communication.&lt;/P&gt;&lt;P&gt;I can get the transmission to work over short distances (&amp;lt;4ft), but once it gets to about 6-8ft, the communication starts to get lost. See the attached oscilloscope plot showing the degradation over about 4 ft of cable. CH2 is on the output of the transmitter and&amp;nbsp; CH1 is at the receiver at the other end of the cable. Seems like the carrier signal is getting washed out a bit over the distance of the cable and I'm not sure why that is happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the amplitude of the carrier signal expected to be so small (~100mV)? I've done simulations of the coupling circuit and it should be much higher (~1.5V).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Dec 2019 21:49:36 GMT</pubDate>
    <dc:creator>roersmat</dc:creator>
    <dc:date>2019-12-13T21:49:36Z</dc:date>
    <item>
      <title>TDA5051A DC Power Line Communication</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TDA5051A-DC-Power-Line-Communication/m-p/980404#M1758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the TDA5051A on a 12VDC power line using the schematic below. 7.372MHz independant oscillator, 115.2kHz carrier frequency. I've tried both 600 and 1200 baud communication.&lt;/P&gt;&lt;P&gt;I can get the transmission to work over short distances (&amp;lt;4ft), but once it gets to about 6-8ft, the communication starts to get lost. See the attached oscilloscope plot showing the degradation over about 4 ft of cable. CH2 is on the output of the transmitter and&amp;nbsp; CH1 is at the receiver at the other end of the cable. Seems like the carrier signal is getting washed out a bit over the distance of the cable and I'm not sure why that is happening.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is the amplitude of the carrier signal expected to be so small (~100mV)? I've done simulations of the coupling circuit and it should be much higher (~1.5V).&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2019 21:49:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TDA5051A-DC-Power-Line-Communication/m-p/980404#M1758</guid>
      <dc:creator>roersmat</dc:creator>
      <dc:date>2019-12-13T21:49:36Z</dc:date>
    </item>
    <item>
      <title>Re: TDA5051A DC Power Line Communication</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TDA5051A-DC-Power-Line-Communication/m-p/980405#M1759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;For your schematic update as below comment then test again:&lt;BR /&gt;1:remove C7/C8&lt;/P&gt;&lt;P&gt;2:use 10uF capacitor connect between L1 and TDA5051 PIN10.&lt;/P&gt;&lt;P&gt;3:use 0.1uF capacitor connect between TDA5051 PIN14 and PIN10.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 05:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TDA5051A-DC-Power-Line-Communication/m-p/980405#M1759</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2019-12-19T05:51:00Z</dc:date>
    </item>
  </channel>
</rss>