<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Relation of Sampling Rate to Tracking Rate in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Relation-of-Sampling-Rate-to-Tracking-Rate/m-p/941224#M1694</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, which device is this question related to?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 11 Oct 2019 08:30:16 GMT</pubDate>
    <dc:creator>davidtosenovjan</dc:creator>
    <dc:date>2019-10-11T08:30:16Z</dc:date>
    <item>
      <title>Relation of Sampling Rate to Tracking Rate</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Relation-of-Sampling-Rate-to-Tracking-Rate/m-p/941223#M1693</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Referring to AN3943. I have the following questions&lt;/P&gt;&lt;P&gt;1. How to convert the position information to digital. Will this conversion lead to truncation errors?&lt;/P&gt;&lt;P&gt;2. Does tracking rate depend on the sampling frequency. For eg For a 12 bit RDC, rollover takes place at 4095 counts/sec for 1 RPS. This means every LSB changes 244us. Could this mean that to detect this change in ATO sampling rate should be atleat 240us or 4Khz?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 10:07:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Relation-of-Sampling-Rate-to-Tracking-Rate/m-p/941223#M1693</guid>
      <dc:creator>garimella</dc:creator>
      <dc:date>2019-10-03T10:07:29Z</dc:date>
    </item>
    <item>
      <title>Re: Relation of Sampling Rate to Tracking Rate</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Relation-of-Sampling-Rate-to-Tracking-Rate/m-p/941224#M1694</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, which device is this question related to?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 11 Oct 2019 08:30:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Relation-of-Sampling-Rate-to-Tracking-Rate/m-p/941224#M1694</guid>
      <dc:creator>davidtosenovjan</dc:creator>
      <dc:date>2019-10-11T08:30:16Z</dc:date>
    </item>
    <item>
      <title>Re: Relation of Sampling Rate to Tracking Rate</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Relation-of-Sampling-Rate-to-Tracking-Rate/m-p/941225#M1695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Referring to AN1942, device 56F80X. I am presuming that sampling frequency should be fast enough to detect the smallest change in the rotor speed. For a 12 bit RDC, speed updation rate is 244us for 60 rpm ( 1rps/4095). Similarly for 10 rps, updation rate would be 24.4us. Here sampling rate must be better that 24 us ( say 20us or 50KHz) to ensure that every delta changes are tracked correctly. Can you clarify if this is true? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Oct 2019 09:22:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Relation-of-Sampling-Rate-to-Tracking-Rate/m-p/941225#M1695</guid>
      <dc:creator>garimella</dc:creator>
      <dc:date>2019-10-26T09:22:51Z</dc:date>
    </item>
  </channel>
</rss>