<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Is there a sample project for the MC56F84789 device that illustrates use of STOP instruction? (Yes, and I include this below) in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-there-a-sample-project-for-the-MC56F84789-device-that/m-p/334008#M169</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the halt and wait are illustrated in the attached zip file which is a zipped project for CodeWarrior 10.6.&lt;/P&gt;&lt;P&gt;It runs on the Tower module for the MC56F84789.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note, most of the work is done with the GUI and Processor Expert.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note that since I used a timer, I can make this time stop or keep running in PEx depending on how I configure the CPU component.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Right now, it is set for keep running.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you make it STOP during STOP mode?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337798"&gt;Haltish.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Sep 2014 00:00:17 GMT</pubDate>
    <dc:creator>johnlwinters</dc:creator>
    <dc:date>2014-09-03T00:00:17Z</dc:date>
    <item>
      <title>Is there a sample project for the MC56F84789 device that illustrates use of STOP instruction? (Yes, and I include this below)</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-there-a-sample-project-for-the-MC56F84789-device-that/m-p/334008#M169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, the halt and wait are illustrated in the attached zip file which is a zipped project for CodeWarrior 10.6.&lt;/P&gt;&lt;P&gt;It runs on the Tower module for the MC56F84789.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note, most of the work is done with the GUI and Processor Expert.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Note that since I used a timer, I can make this time stop or keep running in PEx depending on how I configure the CPU component.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Right now, it is set for keep running.&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you make it STOP during STOP mode?&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337798"&gt;Haltish.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Sep 2014 00:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Is-there-a-sample-project-for-the-MC56F84789-device-that/m-p/334008#M169</guid>
      <dc:creator>johnlwinters</dc:creator>
      <dc:date>2014-09-03T00:00:17Z</dc:date>
    </item>
  </channel>
</rss>