<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic CAN_TX in MPC5746R in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/CAN-TX-in-MPC5746R/m-p/901866#M1640</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem about CAN_TX in MPC5746R.&lt;/P&gt;&lt;P&gt;I wanted to send a sample date but i can't get right date in&amp;nbsp;Oscilloscope.&lt;/P&gt;&lt;P&gt;I didn't know what's wrong. Can someone give me a hand ? thank you very much.&lt;/P&gt;&lt;P&gt;There are my code . Any suggestion is helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt; /* Write your local variable definition here */&lt;/P&gt;&lt;P&gt;#define TX_MAILBOX (1UL)&lt;BR /&gt;#define TX_MSG_ID1 (1UL)&lt;BR /&gt;#define TX_MSG_ID2 (2UL)&lt;BR /&gt;#define RX_MAILBOX (0UL)&lt;BR /&gt;#define RX_MSG_ID1 (2UL)&lt;BR /&gt;#define RX_MSG_ID2 (1UL)&lt;/P&gt;&lt;P&gt;uint8_t TX_date[1];&lt;BR /&gt;uint8_t TX_date1[1];&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,&lt;BR /&gt; g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt;CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;/P&gt;&lt;P&gt;FLEXCAN_DRV_Init(INST_CANCOM1, &amp;amp;canCom1_State, &amp;amp;canCom1_InitConfig0);&lt;BR /&gt;FLEXCAN_DRV_Init(INST_CANCOM2, &amp;amp;canCom2_State, &amp;amp;canCom2_InitConfig0);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;flexcan_data_info_t dataInfo =&lt;BR /&gt; {&lt;BR /&gt; .data_length = 1UL,&lt;BR /&gt; .msg_id_type = FLEXCAN_MSG_ID_STD&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Configure TX message buffer with index TX_MSG_ID1 and TX_MAILBOX*/&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID1);&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM2, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID2);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;while(1)&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TX_date[0] = 0x11U;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Execute send non-blocking */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; FLEXCAN_DRV_Send(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID1, (uint8_t*)TX_date);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80497i2B8544A25BA1C6C2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 May 2019 04:20:50 GMT</pubDate>
    <dc:creator>dreamtea81125</dc:creator>
    <dc:date>2019-05-06T04:20:50Z</dc:date>
    <item>
      <title>CAN_TX in MPC5746R</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/CAN-TX-in-MPC5746R/m-p/901866#M1640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem about CAN_TX in MPC5746R.&lt;/P&gt;&lt;P&gt;I wanted to send a sample date but i can't get right date in&amp;nbsp;Oscilloscope.&lt;/P&gt;&lt;P&gt;I didn't know what's wrong. Can someone give me a hand ? thank you very much.&lt;/P&gt;&lt;P&gt;There are my code . Any suggestion is helpful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt; /* Write your local variable definition here */&lt;/P&gt;&lt;P&gt;#define TX_MAILBOX (1UL)&lt;BR /&gt;#define TX_MSG_ID1 (1UL)&lt;BR /&gt;#define TX_MSG_ID2 (2UL)&lt;BR /&gt;#define RX_MAILBOX (0UL)&lt;BR /&gt;#define RX_MSG_ID1 (2UL)&lt;BR /&gt;#define RX_MSG_ID2 (1UL)&lt;/P&gt;&lt;P&gt;uint8_t TX_date[1];&lt;BR /&gt;uint8_t TX_date1[1];&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,&lt;BR /&gt; g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt;CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;/P&gt;&lt;P&gt;FLEXCAN_DRV_Init(INST_CANCOM1, &amp;amp;canCom1_State, &amp;amp;canCom1_InitConfig0);&lt;BR /&gt;FLEXCAN_DRV_Init(INST_CANCOM2, &amp;amp;canCom2_State, &amp;amp;canCom2_InitConfig0);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;flexcan_data_info_t dataInfo =&lt;BR /&gt; {&lt;BR /&gt; .data_length = 1UL,&lt;BR /&gt; .msg_id_type = FLEXCAN_MSG_ID_STD&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Configure TX message buffer with index TX_MSG_ID1 and TX_MAILBOX*/&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID1);&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM2, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID2);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;while(1)&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;TX_date[0] = 0x11U;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Execute send non-blocking */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; FLEXCAN_DRV_Send(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID1, (uint8_t*)TX_date);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80497i2B8544A25BA1C6C2/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 May 2019 04:20:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/CAN-TX-in-MPC5746R/m-p/901866#M1640</guid>
      <dc:creator>dreamtea81125</dc:creator>
      <dc:date>2019-05-06T04:20:50Z</dc:date>
    </item>
  </channel>
</rss>