<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Re: ticket</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901830#M1636</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you use EVB on your side? Seems you are using 2 FlexCAN modules, do you want to do communication between those 2? If yes, how those modules are connected together?&lt;/P&gt;&lt;P&gt;Regarding a code; it is not needed to call&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;FLEXCAN_DRV_ConfigTxMb() each time you want to send message.&amp;nbsp;You have placed this in main's while loop. Also calling non-blocking&amp;nbsp;&lt;SPAN&gt;FLEXCAN_DRV_Send() periodically is not correct. You have to be sure previous transmission is finished. FLEXCAN_DRV_GetTransferStatus() can be used for this.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 06 May 2019 11:32:31 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2019-05-06T11:32:31Z</dc:date>
    <item>
      <title>ticket</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901829#M1635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have some problem about CAN_TX in MPC5746R.&lt;/P&gt;&lt;P&gt;there are my code and i can't get the right date in&amp;nbsp;Oscilloscope.&lt;/P&gt;&lt;P&gt;I didn't know what's wrong. Can someone give me a hand?&amp;nbsp; &amp;nbsp;thank you very much.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int main(void)&lt;/P&gt;&lt;P&gt;{&lt;BR /&gt; /* Write your local variable definition here */&lt;/P&gt;&lt;P&gt;#define TX_MAILBOX (1UL)&lt;BR /&gt;#define TX_MSG_ID1 (1UL)&lt;BR /&gt;#define TX_MSG_ID2 (2UL)&lt;BR /&gt;#define RX_MAILBOX (0UL)&lt;BR /&gt;#define RX_MSG_ID1 (2UL)&lt;BR /&gt;#define RX_MSG_ID2 (1UL)&lt;/P&gt;&lt;P&gt;uint8_t TX_date[1];&lt;BR /&gt;uint8_t TX_date1[1];&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt;CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;/P&gt;&lt;P&gt;FLEXCAN_DRV_Init(INST_CANCOM1, &amp;amp;canCom1_State, &amp;amp;canCom1_InitConfig0);&lt;BR /&gt;FLEXCAN_DRV_Init(INST_CANCOM2, &amp;amp;canCom2_State, &amp;amp;canCom2_InitConfig0);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;flexcan_data_info_t dataInfo =&lt;BR /&gt; {&lt;BR /&gt; .data_length = 1UL,&lt;BR /&gt; .msg_id_type = FLEXCAN_MSG_ID_STD&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /* Configure RX message buffer with index RX_MSG_ID and RX_MAILBOX */&lt;BR /&gt; FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, RX_MAILBOX, &amp;amp;dataInfo, RX_MSG_ID1);&lt;BR /&gt; FLEXCAN_DRV_ConfigRxMb(INST_CANCOM2, RX_MAILBOX, &amp;amp;dataInfo, RX_MSG_ID2);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;while(1)&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Configure TX message buffer with index TX_MSG_ID1 and TX_MAILBOX*/&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID1);&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM2, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID2);&lt;BR /&gt;&lt;BR /&gt; TX_date[0] = 0x11U;&lt;/P&gt;&lt;P&gt;/* Execute send non-blocking */&lt;BR /&gt; FLEXCAN_DRV_Send(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID1, (uint8_t*)TX_date);&lt;BR /&gt;&lt;BR /&gt;// FLEXCAN_DRV_Send(INST_CANCOM2, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID2, &amp;amp;TX_date1);&lt;/P&gt;&lt;P&gt;// FLEXCAN_DRV_SendBlocking(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID2, &amp;amp;TX_date, 200);&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/80800i5DAB65ED3095E23C/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 May 2019 03:26:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901829#M1635</guid>
      <dc:creator>dreamtea81125</dc:creator>
      <dc:date>2019-05-06T03:26:09Z</dc:date>
    </item>
    <item>
      <title>Re: ticket</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901830#M1636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;do you use EVB on your side? Seems you are using 2 FlexCAN modules, do you want to do communication between those 2? If yes, how those modules are connected together?&lt;/P&gt;&lt;P&gt;Regarding a code; it is not needed to call&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;FLEXCAN_DRV_ConfigTxMb() each time you want to send message.&amp;nbsp;You have placed this in main's while loop. Also calling non-blocking&amp;nbsp;&lt;SPAN&gt;FLEXCAN_DRV_Send() periodically is not correct. You have to be sure previous transmission is finished. FLEXCAN_DRV_GetTransferStatus() can be used for this.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 May 2019 11:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901830#M1636</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-05-06T11:32:31Z</dc:date>
    </item>
    <item>
      <title>Re: ticket</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901831#M1637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Hi, Petr Stancik&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Thank you for your respond.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;Yes. I use EVB on my side.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;I can send the data by EVB and get the data by CAN converter in computer new.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;but it seem have some problems. I can't receive the data by EVB.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;I don't know what's wrong. Can you give some advice.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.5pt; color: #3d3d3d;"&gt;There are my code . Any suggestion is helpful.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;int main(void)&lt;BR /&gt;{&lt;BR /&gt; /* Write your local variable definition here */&lt;/P&gt;&lt;P&gt;#define TX_MAILBOX (1UL)&lt;BR /&gt;#define TX_MSG_ID1 (1UL)&lt;BR /&gt;#define TX_MSG_ID2 (2UL)&lt;BR /&gt;#define RX_MAILBOX (0UL)&lt;BR /&gt;#define RX_MSG_ID1 (2UL)&lt;BR /&gt;#define RX_MSG_ID2 (1UL)&lt;/P&gt;&lt;P&gt;uint8_t TX_date = 0x52U;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/&lt;BR /&gt; #ifdef PEX_RTOS_INIT&lt;BR /&gt; PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */&lt;BR /&gt; #endif&lt;BR /&gt; /*** End of Processor Expert internal initialization. ***/&lt;/P&gt;&lt;P&gt;/* Write your code here */&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,&lt;BR /&gt; g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);&lt;BR /&gt;CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_FORCIBLE);&lt;/P&gt;&lt;P&gt;PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);&lt;/P&gt;&lt;P&gt;FLEXCAN_DRV_Init(INST_CANCOM1, &amp;amp;canCom1_State, &amp;amp;canCom1_InitConfig0);&lt;BR /&gt;FLEXCAN_DRV_Init(INST_CANCOM2, &amp;amp;canCom2_State, &amp;amp;canCom2_InitConfig0);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;flexcan_data_info_t dataInfo =&lt;BR /&gt; {&lt;BR /&gt; .data_length = 1U,&lt;BR /&gt; .msg_id_type = FLEXCAN_MSG_ID_STD&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /* Configure RX message buffer with index RX_MSG_ID and RX_MAILBOX */&lt;BR /&gt; FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, RX_MAILBOX, &amp;amp;dataInfo, RX_MSG_ID1);&lt;BR /&gt; FLEXCAN_DRV_ConfigRxMb(INST_CANCOM2, RX_MAILBOX, &amp;amp;dataInfo, RX_MSG_ID2);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /* Configure TX message buffer with index TX_MSG_ID1 and TX_MAILBOX*/&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID1);&lt;BR /&gt; FLEXCAN_DRV_ConfigTxMb(INST_CANCOM2, TX_MAILBOX, &amp;amp;dataInfo, TX_MSG_ID2);&lt;/P&gt;&lt;P&gt;PINS_DRV_SetPins(PTA,3U);&lt;BR /&gt; PINS_DRV_GetPinsOutput(PTA);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;while(1)&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /* Execute send non-blocking */&lt;BR /&gt; FLEXCAN_DRV_Send(INST_CANCOM1, TX_MAILBOX, &amp;amp;dataInfo, 2UL, &amp;amp;TX_date);&lt;/P&gt;&lt;P&gt;// FLEXCAN_DRV_Send(INST_CANCOM2, TX_MAILBOX, &amp;amp;dataInfo, 1UL, &amp;amp;TX_date1);&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; /* Define receive buffer */&lt;BR /&gt; flexcan_msgbuff_t recvBuff;&lt;BR /&gt; flexcan_msgbuff_t recvBuff1;&lt;BR /&gt; recvBuff1.msgId=1U;&lt;BR /&gt; recvBuff1.dataLen=8U;&lt;/P&gt;&lt;P&gt;/* Start receiving data in RX_MAILBOX. */&lt;/P&gt;&lt;P&gt;FLEXCAN_DRV_ReceiveBlocking(INST_CANCOM2,RX_MAILBOX, &amp;amp;recvBuff1,200);&lt;BR /&gt;// FLEXCAN_DRV_Receive(INST_CANCOM2,RX_MAILBOX, &amp;amp;recvBuff1);&lt;BR /&gt; if(recvBuff1.data[0]==1)&lt;BR /&gt; {&lt;/P&gt;&lt;P&gt;PINS_DRV_WritePin(PTA,3U,1U);&lt;BR /&gt; }&lt;BR /&gt;// FLEXCAN_DRV_Receive(INST_CANCOM1,RX_MAILBOX, &amp;amp;recvBuff);&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/76835i8BD56773E0F8B5C5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 08:50:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901831#M1637</guid>
      <dc:creator>dreamtea81125</dc:creator>
      <dc:date>2019-05-08T08:50:21Z</dc:date>
    </item>
    <item>
      <title>Re: ticket</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901832#M1638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This is my setting in can converter. Thank you.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79474iDD01D82FD1D5D3CD/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79906iC84965603F006E64/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2019 09:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901832#M1638</guid>
      <dc:creator>dreamtea81125</dc:creator>
      <dc:date>2019-05-08T09:01:03Z</dc:date>
    </item>
    <item>
      <title>Re: ticket</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901833#M1639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you can use below code to receive a message&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;flexcan_data_info_t dataInfo =&lt;BR /&gt; {&lt;BR /&gt; .data_length = 1U,&lt;BR /&gt; .msg_id_type = FLEXCAN_MSG_ID_STD&lt;BR /&gt; };&lt;/P&gt;&lt;P&gt;/* Configure RX message buffer with index RX_MSG_ID and RX_MAILBOX */&lt;BR /&gt; FLEXCAN_DRV_ConfigRxMb(INST_CANCOM1, RX_MAILBOX, &amp;amp;dataInfo, RX_MSG_ID1);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;while(1)&lt;BR /&gt; {&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;/* Define receive buffer */&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;flexcan_msgbuff_t recvBuff;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;/* Start receiving data in RX_MAILBOX. */&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;FLEXCAN_DRV_Receive(INST_CANCOM1, RX_MAILBOX, &amp;amp;recvBuff);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;/* Wait until the previous FlexCAN receive is completed */&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;while((FLEXCAN_DRV_GetTransferStatus(INST_CANCOM1, RX_MAILBOX) == STATUS_BUSY);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;/* Check the received message ID and payload */&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;....&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also you set bitrate to 10kbps in flexcan components. This is quite low one. How this can work&amp;nbsp;as EVB is using TJA1041 which has minimum possible bitrate of 40kbps (due to TXD dominant clamping detection)?&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Moreover the CAN bit setting of the PC tool is weird, 10K is selected and it shows 83.333 kbps.&lt;/P&gt;&lt;P&gt;So do you have really same bitrate set on MCU and PC side? The same sample point is also recommended.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR, Petr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 May 2019 11:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/ticket/m-p/901833#M1639</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2019-05-09T11:33:01Z</dc:date>
    </item>
  </channel>
</rss>