<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: TJA1051T/3 internal pull down resistor on pin S</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886799#M1590</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Savic,&lt;/P&gt;&lt;P&gt;Generally, the pull-down resistor is about 20K to 50K ohm. You can connect the pin with push-pull GPIO pin of mcu to the S or EN pins of the TJA1051T/3.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;H1&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Mar 2019 03:26:10 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-03-13T03:26:10Z</dc:date>
    <item>
      <title>TJA1051T/3 internal pull down resistor on pin S</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886798#M1589</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently dealing with the CAN transceiver TJA1051T/3. It has pin named S which is used to bring the transceiver in Normal or Silent mode. I am not sure if I am correct but I think the transceiver should stay Silent until the MCU activates it by setting pin S low. However, S pin has internal pull down resistor which brings it in Normal mode by default. Since the MCU I am using has no pull up or pull down enabled in the first place, it will allow internal pull down to dominate.&lt;/P&gt;&lt;P&gt;My question is what is the value of the internal pull down resistor inside the S pin of the TJA1051T/3?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 10:43:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886798#M1589</guid>
      <dc:creator>nexy_sm</dc:creator>
      <dc:date>2019-03-12T10:43:16Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1051T/3 internal pull down resistor on pin S</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886799#M1590</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Savic,&lt;/P&gt;&lt;P&gt;Generally, the pull-down resistor is about 20K to 50K ohm. You can connect the pin with push-pull GPIO pin of mcu to the S or EN pins of the TJA1051T/3.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;H1&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Mar 2019 03:26:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886799#M1590</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-03-13T03:26:10Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1051T/3 internal pull down resistor on pin S</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886800#M1591</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Rong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;there will be a short glitch between the POR and pin configuration during which the CAN transceiver is enabled. This is something I would like to avoid although it is not that critical in my opinion. I also wonder why they included internal pull downs instead of pull ups.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Mar 2019 09:39:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886800#M1591</guid>
      <dc:creator>nexy_sm</dc:creator>
      <dc:date>2019-03-13T09:39:23Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1051T/3 internal pull down resistor on pin S</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886801#M1592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Nemanja,&lt;/P&gt;&lt;P&gt;Regarding the question why they included internal pull downs instead of pull ups, assume the scenario that the processor connected to the CAN transceiver TJA1051T/3 is power off, but the TJA1051T/3 is powered up, because the CAN bus is network connection, in the case, EN is low, S is low, the CAN driver pin CAN_H and CAN_L are float, so the node with TJA1051T/3 does not take effect on the CAN bus, in other words, the CAN bus can work although the node of TJA1051T/3 does not work.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2019 02:50:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886801#M1592</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-03-14T02:50:38Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1051T/3 internal pull down resistor on pin S</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886802#M1593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my case, I use TJA1051T/3, so EN pin is internally connected with Vcc. This means as far as I could understand that, in order to go silent S needs to be high, but it is internally pulled to low.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 Mar 2019 14:35:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886802#M1593</guid>
      <dc:creator>nexy_sm</dc:creator>
      <dc:date>2019-03-14T14:35:35Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1051T/3 internal pull down resistor on pin S</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886803#M1594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Savic,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to control TJA1051T/3 to enable or disable even silent/ normal mode, you can connect the MCU GPIO pins to the EN/S pins. If you do not want to control them, you can connect external pull-up resistor for example1K ohm to the EN or S pin based on your requirement.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2019 02:44:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TJA1051T-3-internal-pull-down-resistor-on-pin-S/m-p/886803#M1594</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-03-15T02:44:54Z</dc:date>
    </item>
  </channel>
</rss>