<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックSC16IS741A Default behavior</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC16IS741A-Default-behavior/m-p/853195#M1445</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I try to figure out what's the factory default behavior of the SC16IS741A chip, without any configuration encoded whatsoever, in SPI mode.&lt;/P&gt;&lt;P&gt;- First will it be usable as is, with factory default? Or am I forced to encode configuration setting registers to make it work? (Assuming default settings are OK for my application)&lt;BR /&gt;And if yes what will do basically, in SPI mode.&lt;/P&gt;&lt;P&gt;- Is the default word format is 8N1. The datasheet indicates that "no parity" is "default normal condition". But it doesn't indicates the default condition for the stop bit (Is it 1 or 2?).&lt;BR /&gt;It would be 0-1 if LCR[2] default is 0. (how could it be without stop bit ???)&lt;BR /&gt;And it doesn't indicate the default value for the word length. Here, if the value in LCR[1] and [0] the word length would 5, which is very strange.&lt;BR /&gt;So, what are the default values for LCR[2],[1] and [0]?&lt;/P&gt;&lt;P&gt;- In SPI mode, as FIFO is left disabled by default, is it necessary to send a read request ("10000000" followed by the response) or would data flow automatically from RX to SO?&lt;BR /&gt;And vice versa: Would it be necessary to send a write request instead of just feeding the data through the circuit?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Jan 2019 19:14:38 GMT</pubDate>
    <dc:creator>projects1</dc:creator>
    <dc:date>2019-01-22T19:14:38Z</dc:date>
    <item>
      <title>SC16IS741A Default behavior</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC16IS741A-Default-behavior/m-p/853195#M1445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello. I try to figure out what's the factory default behavior of the SC16IS741A chip, without any configuration encoded whatsoever, in SPI mode.&lt;/P&gt;&lt;P&gt;- First will it be usable as is, with factory default? Or am I forced to encode configuration setting registers to make it work? (Assuming default settings are OK for my application)&lt;BR /&gt;And if yes what will do basically, in SPI mode.&lt;/P&gt;&lt;P&gt;- Is the default word format is 8N1. The datasheet indicates that "no parity" is "default normal condition". But it doesn't indicates the default condition for the stop bit (Is it 1 or 2?).&lt;BR /&gt;It would be 0-1 if LCR[2] default is 0. (how could it be without stop bit ???)&lt;BR /&gt;And it doesn't indicate the default value for the word length. Here, if the value in LCR[1] and [0] the word length would 5, which is very strange.&lt;BR /&gt;So, what are the default values for LCR[2],[1] and [0]?&lt;/P&gt;&lt;P&gt;- In SPI mode, as FIFO is left disabled by default, is it necessary to send a read request ("10000000" followed by the response) or would data flow automatically from RX to SO?&lt;BR /&gt;And vice versa: Would it be necessary to send a write request instead of just feeding the data through the circuit?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Jan 2019 19:14:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SC16IS741A-Default-behavior/m-p/853195#M1445</guid>
      <dc:creator>projects1</dc:creator>
      <dc:date>2019-01-22T19:14:38Z</dc:date>
    </item>
  </channel>
</rss>