<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TDM/I2S communication to TFA9896 in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TDM-I2S-communication-to-TFA9896/m-p/829437#M1388</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the TFA9896 to collect audio&amp;nbsp;signals over the I2S line, but the collected data sounds really lousy.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;transmitting device has a Clock on 256kHz, and a Frame Sync on 8kHz.&lt;/P&gt;&lt;P&gt;The TFA9896 collects data with a Clock on 1.536MHz, and a Frame Sync on 48kHz.&lt;/P&gt;&lt;P&gt;I am collecting signals on&amp;nbsp;the TFA's "I2S IN1" line with their corresponding BCK, WS and DATA pins.&lt;/P&gt;&lt;P&gt;I should be able to change the Sync frequency on the TFA9896 with I2C, by sending 0x00 &amp;amp; 0x90 to address 0x04, but when I change the configurations as the datasheet says, it doesn't seem to change the actual Sync frequency at all when I measure the signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I using the correct I2S inputs pins, or are there pins designed for the TDM configurations?&lt;/P&gt;&lt;P&gt;Am I using the correct configurations to change the frequencies?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Oct 2018 11:50:59 GMT</pubDate>
    <dc:creator>morten</dc:creator>
    <dc:date>2018-10-24T11:50:59Z</dc:date>
    <item>
      <title>TDM/I2S communication to TFA9896</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/TDM-I2S-communication-to-TFA9896/m-p/829437#M1388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the TFA9896 to collect audio&amp;nbsp;signals over the I2S line, but the collected data sounds really lousy.&lt;/P&gt;&lt;P&gt;The&amp;nbsp;transmitting device has a Clock on 256kHz, and a Frame Sync on 8kHz.&lt;/P&gt;&lt;P&gt;The TFA9896 collects data with a Clock on 1.536MHz, and a Frame Sync on 48kHz.&lt;/P&gt;&lt;P&gt;I am collecting signals on&amp;nbsp;the TFA's "I2S IN1" line with their corresponding BCK, WS and DATA pins.&lt;/P&gt;&lt;P&gt;I should be able to change the Sync frequency on the TFA9896 with I2C, by sending 0x00 &amp;amp; 0x90 to address 0x04, but when I change the configurations as the datasheet says, it doesn't seem to change the actual Sync frequency at all when I measure the signals.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I using the correct I2S inputs pins, or are there pins designed for the TDM configurations?&lt;/P&gt;&lt;P&gt;Am I using the correct configurations to change the frequencies?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2018 11:50:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/TDM-I2S-communication-to-TFA9896/m-p/829437#M1388</guid>
      <dc:creator>morten</dc:creator>
      <dc:date>2018-10-24T11:50:59Z</dc:date>
    </item>
  </channel>
</rss>