<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re:  SC18IM700 (UART / I2C bridge) in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IM700-UART-I2C-bridge/m-p/820545#M1381</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In SC18IM700.pdf Section 2&amp;nbsp;there is a generic description stating&amp;nbsp; "2.4 V and 3.6 V operation"; that's Vdd range.&lt;BR /&gt;SC18IM700 is also "5V tolerant on the INPUT pins".&lt;BR /&gt;&lt;BR /&gt;More details are given in&amp;nbsp;section 11 "Static characteristics"::&lt;BR /&gt;"Vdd = 2.4 V to 3.6 V; T amb = +40°C to +85°C; unless otherwise specified."&lt;BR /&gt;&lt;BR /&gt;Also from Section 11, looking at Vil and Voh specifications,&amp;nbsp; the "5V tolerant on the input pins" translates into&lt;BR /&gt;"completely 5V input tolerant for SDA and SCL ONLY"&lt;BR /&gt;because&amp;nbsp; their input voltage ranges from -0.5V to 5.5V (REFERENCED TO Vss), with thresholds at 0.3Vdd and 0.7Vdd.&lt;BR /&gt;&lt;BR /&gt;GPIOs are 5V tolerant too, but with a very important CAVEAT to remember:&lt;BR /&gt;in section 9.2.2.1 there is a warning about them when used in quasi-bidirectional mode with 5V inputs that says&lt;BR /&gt;"The SC18IM700 is a 3 V device, but the pins are 5 V tolerant. In&amp;nbsp;QUASI-BIDIRECTIONAL mode,&lt;BR /&gt;if a user applies 5 V on the pin, there will be a current flowing from the pin to Vdd , causing&lt;BR /&gt;EXTRA POWER CONSUMPTION. Therefore, applying 5 V in quasi-bidirectional mode is&lt;BR /&gt;discouraged."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 29 Jun 2020 10:29:14 GMT</pubDate>
    <dc:creator>Lorenzo_Mch_IT</dc:creator>
    <dc:date>2020-06-29T10:29:14Z</dc:date>
    <item>
      <title>SC18IM700 (UART / I2C bridge)</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IM700-UART-I2C-bridge/m-p/820543#M1379</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp; &lt;/P&gt;&lt;P&gt;The DS of the chip SC18IM700 (UART / I2C bridge)&amp;nbsp; contains&amp;nbsp; no limiting values for Vdd (or I couldn't find any). Please answer: &lt;BR /&gt;1. Can the chip function when Vdd is between 3.9 - 5.0 V ?&lt;BR /&gt;2. Table 11 in the Datasheet contain Limiting value for an "input voltage" only.&amp;nbsp;&amp;nbsp; What does this "input" mean - Tx and Rx only, or SDA and GPIOx also (these can be programmed for input)? &amp;nbsp;&lt;BR /&gt;Thanx!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Nov 2018 23:48:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IM700-UART-I2C-bridge/m-p/820543#M1379</guid>
      <dc:creator>pdemcenko</dc:creator>
      <dc:date>2018-11-29T23:48:11Z</dc:date>
    </item>
    <item>
      <title>Re:  SC18IM700 (UART / I2C bridge)</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IM700-UART-I2C-bridge/m-p/820544#M1380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same question. I have to interface with an I2C device that uses 5V levels.&lt;/P&gt;&lt;P&gt;The SC18IM700 is not interpretting the acknolegment as its Vil = 0.3 * Vdd. Can i operate the SC18IM700 from 5V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Cheers&lt;/P&gt;&lt;P&gt;G&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2020 09:24:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IM700-UART-I2C-bridge/m-p/820544#M1380</guid>
      <dc:creator>graeme_anderson</dc:creator>
      <dc:date>2020-06-29T09:24:11Z</dc:date>
    </item>
    <item>
      <title>Re:  SC18IM700 (UART / I2C bridge)</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IM700-UART-I2C-bridge/m-p/820545#M1381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In SC18IM700.pdf Section 2&amp;nbsp;there is a generic description stating&amp;nbsp; "2.4 V and 3.6 V operation"; that's Vdd range.&lt;BR /&gt;SC18IM700 is also "5V tolerant on the INPUT pins".&lt;BR /&gt;&lt;BR /&gt;More details are given in&amp;nbsp;section 11 "Static characteristics"::&lt;BR /&gt;"Vdd = 2.4 V to 3.6 V; T amb = +40°C to +85°C; unless otherwise specified."&lt;BR /&gt;&lt;BR /&gt;Also from Section 11, looking at Vil and Voh specifications,&amp;nbsp; the "5V tolerant on the input pins" translates into&lt;BR /&gt;"completely 5V input tolerant for SDA and SCL ONLY"&lt;BR /&gt;because&amp;nbsp; their input voltage ranges from -0.5V to 5.5V (REFERENCED TO Vss), with thresholds at 0.3Vdd and 0.7Vdd.&lt;BR /&gt;&lt;BR /&gt;GPIOs are 5V tolerant too, but with a very important CAVEAT to remember:&lt;BR /&gt;in section 9.2.2.1 there is a warning about them when used in quasi-bidirectional mode with 5V inputs that says&lt;BR /&gt;"The SC18IM700 is a 3 V device, but the pins are 5 V tolerant. In&amp;nbsp;QUASI-BIDIRECTIONAL mode,&lt;BR /&gt;if a user applies 5 V on the pin, there will be a current flowing from the pin to Vdd , causing&lt;BR /&gt;EXTRA POWER CONSUMPTION. Therefore, applying 5 V in quasi-bidirectional mode is&lt;BR /&gt;discouraged."&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Jun 2020 10:29:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SC18IM700-UART-I2C-bridge/m-p/820545#M1381</guid>
      <dc:creator>Lorenzo_Mch_IT</dc:creator>
      <dc:date>2020-06-29T10:29:14Z</dc:date>
    </item>
  </channel>
</rss>