<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using the PN5180 with Balun in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Using-the-PN5180-with-Balun/m-p/805847#M1349</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good Morning Guys,&lt;/P&gt;&lt;P&gt;in a new little project we want to use the PN5180 with a extended antenna. This should be realized over a Balun after the EMC network.&lt;/P&gt;&lt;P&gt;We found some examples which are really helpfully for using the CLRC663 because it only has one RX Pin. But what should we do with the second Rx Pin of the PN5180? is there a register to use both or is it only regulated by the AGC (Page 79 in the Datasheet).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish you a wonderful day :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Aug 2018 06:59:54 GMT</pubDate>
    <dc:creator>berndbogenriede</dc:creator>
    <dc:date>2018-08-01T06:59:54Z</dc:date>
    <item>
      <title>Using the PN5180 with Balun</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Using-the-PN5180-with-Balun/m-p/805847#M1349</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good Morning Guys,&lt;/P&gt;&lt;P&gt;in a new little project we want to use the PN5180 with a extended antenna. This should be realized over a Balun after the EMC network.&lt;/P&gt;&lt;P&gt;We found some examples which are really helpfully for using the CLRC663 because it only has one RX Pin. But what should we do with the second Rx Pin of the PN5180? is there a register to use both or is it only regulated by the AGC (Page 79 in the Datasheet).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Wish you a wonderful day :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 06:59:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Using-the-PN5180-with-Balun/m-p/805847#M1349</guid>
      <dc:creator>berndbogenriede</dc:creator>
      <dc:date>2018-08-01T06:59:54Z</dc:date>
    </item>
  </channel>
</rss>