<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: USB Programmer for DSP56807</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802827#M1337</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have never tried downloading code using just a .S file.&amp;nbsp; I always have had the full set of code in the project.&lt;/P&gt;&lt;P&gt;I am not familiar with what files the debugger needs to be able to download code from a .S file if it even can.&lt;/P&gt;&lt;P&gt;Maybe someone else is more familiar with that.&lt;/P&gt;&lt;P&gt;Do you have any backup of the CW project and the CW version that it was created under?&amp;nbsp; That may be the best alternative.&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 28 Nov 2018 15:47:25 GMT</pubDate>
    <dc:creator>dynapb</dc:creator>
    <dc:date>2018-11-28T15:47:25Z</dc:date>
    <item>
      <title>USB Programmer for DSP56807</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802824#M1334</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need a USB programmer for the &lt;STRONG&gt;DSP56807&lt;/STRONG&gt; device.&lt;/P&gt;&lt;P&gt;Until now I used a parallel port programmer, but we no longer have PCs with this interface or the parallel port cards in Windows 7 or 10 do not work.&lt;/P&gt;&lt;P&gt;We have acquired the CodeWarrior &lt;STRONG&gt;USB TAP programmer&lt;/STRONG&gt; and we thought that with the &lt;STRONG&gt;Flash Programmer&lt;/STRONG&gt; tool it would work, but it seems that it only supports DSP 56800E.&lt;/P&gt;&lt;P&gt;In some forums, they indicate that from the Codewarrior software the DSP56807 can be programmed with the USB TAP programmer, but we do not see how it works.&lt;/P&gt;&lt;P&gt;We need a solution, since in the production plant we are almost without resources to be able to record.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;P&gt;Greetings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Nov 2018 16:08:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802824#M1334</guid>
      <dc:creator>javmol</dc:creator>
      <dc:date>2018-11-26T16:08:48Z</dc:date>
    </item>
    <item>
      <title>Re: USB Programmer for DSP56807</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802825#M1335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jav&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only way I know of to program the 56F807 using the USB TAP is through the CW Classic IDE.&amp;nbsp; That is very slow but works.&amp;nbsp; I use the Classic IDE on Win7.&lt;/P&gt;&lt;P&gt;The 807 website shows the Flash Programming Tool for the 807 from the Eclipse IDE but I have never used it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have a serial interface going to SCI0 on the 807?&amp;nbsp; If so you can download code using the serial bootloader and that is much faster and is the way we do it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 15:35:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802825#M1335</guid>
      <dc:creator>dynapb</dc:creator>
      <dc:date>2018-11-27T15:35:14Z</dc:date>
    </item>
    <item>
      <title>Re: USB Programmer for DSP56807</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802826#M1336</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;It is an old design, which is not possible to redesign to add the option of loading through bootloader, it is necessary to maintain compatibility and support with everything supplied to our customers.&lt;BR /&gt;I have the "CodeWarrior for 56800E Digital Signal Controllers v8.3" installed, but it is an environment that I do not know and I do not find the option to program through the USP-TAP, until now the files we used were with extension ".s" + ".cfg" configuration and we loaded them using the "flash_over_jtag.exe" through the parallel port; I think, to use the CodeWarrior, the files with extension ".elf" are necessary, is that so ?, could you indicate me what is the way to record through the CodeWarrior.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Regards and thanks for everything.&lt;/DIV&gt;&lt;DIV&gt;Javier.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Nov 2018 16:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802826#M1336</guid>
      <dc:creator>javmol</dc:creator>
      <dc:date>2018-11-27T16:58:56Z</dc:date>
    </item>
    <item>
      <title>Re: USB Programmer for DSP56807</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802827#M1337</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have never tried downloading code using just a .S file.&amp;nbsp; I always have had the full set of code in the project.&lt;/P&gt;&lt;P&gt;I am not familiar with what files the debugger needs to be able to download code from a .S file if it even can.&lt;/P&gt;&lt;P&gt;Maybe someone else is more familiar with that.&lt;/P&gt;&lt;P&gt;Do you have any backup of the CW project and the CW version that it was created under?&amp;nbsp; That may be the best alternative.&lt;/P&gt;&lt;P&gt;Pete&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 15:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802827#M1337</guid>
      <dc:creator>dynapb</dc:creator>
      <dc:date>2018-11-28T15:47:25Z</dc:date>
    </item>
    <item>
      <title>Re: USB Programmer for DSP56807</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802828#M1338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I'm going to try to generate a .elf file and try from codewarrior.&lt;/DIV&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;Thanks for your help&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Nov 2018 16:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/USB-Programmer-for-DSP56807/m-p/802828#M1338</guid>
      <dc:creator>javmol</dc:creator>
      <dc:date>2018-11-28T16:25:11Z</dc:date>
    </item>
  </channel>
</rss>