<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: What is the maximum I/O source current per bit for the PCA9698? in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798283#M1313</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I think that you are right. Thank you very much for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Manuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Fri, Aug 10, 2018 at 11:32 AM, xiangjun.rong &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 Aug 2018 10:10:28 GMT</pubDate>
    <dc:creator>manuelcaracuel</dc:creator>
    <dc:date>2018-08-10T10:10:28Z</dc:date>
    <item>
      <title>What is the maximum I/O source current per bit for the PCA9698?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798278#M1308</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to use the GPIO expander for I2C&amp;nbsp;bus&amp;nbsp;PCA9698, but I have some limitations of power. At the beginning of the datasheet, it says that&amp;nbsp;at 5 V supply voltage, the outputs are capable of sourcing 10 mA and sinking 25 mA with a total package load of 1 A.&amp;nbsp;Does this mean that the maximum current that can source is 10 mA at 5V supply voltage? Because at the end of the document, appear a graphic that indicates to me that the maximum output source current is greater than 10 mA in some conditions.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/73146i60DE235542F3627E/image-size/large?v=v2&amp;amp;px=999" title="Screen Shot 2018-07-30 at 13.08.46.png" alt="Screen Shot 2018-07-30 at 13.08.46.png" /&gt;&lt;/span&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the answer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 11:25:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798278#M1308</guid>
      <dc:creator>manuelcaracuel</dc:creator>
      <dc:date>2018-07-30T11:25:11Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum I/O source current per bit for the PCA9698?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798279#M1309</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Manuel,&lt;/P&gt;&lt;P&gt;Frankly speaking, this is DSC forum, PCA9698 does not belong to DSC family. But your question is a general one, I can help answer it here.&lt;/P&gt;&lt;P&gt;The data sheet&amp;nbsp; says that&amp;nbsp;at 5 V supply voltage, the outputs are capable of sourcing 10 mA and sinking 25 mA with a total package load of 1 A.&lt;/P&gt;&lt;P&gt;From the Fig34 you posted, the GPIO pin can output current more than 10mA, it can reach up to the 40mA for the temperature 25 degree curve, in the case, the VDD-VOH is 0.6V, in other words, if the rail voltage is 5V, the pin output voltage/current is 4.4V/40mA.&amp;nbsp; If the current is 10mA, the pin output voltage/current is 4.9V/10mA.&lt;/P&gt;&lt;P&gt;The Data sheet says that if each GPIO pins output current is less than 10mA, we can guarantee the total package load of 1 A. But if the pin current is out of the range, the total package load may excess 1A.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2018 06:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798279#M1309</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-08-02T06:20:08Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum I/O source current per bit for the PCA9698?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798280#M1310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you so much Xiangjun for you answer. You helped me a lot.&lt;/P&gt;&lt;P&gt;Manuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Aug 2018 07:13:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798280#M1310</guid>
      <dc:creator>manuelcaracuel</dc:creator>
      <dc:date>2018-08-02T07:13:17Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum I/O source current per bit for the PCA9698?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798281#M1311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi again Xiangjun,&lt;/P&gt;&lt;P&gt;I'm sorry to have to write again but I have read your answer again and&lt;/P&gt;&lt;P&gt;there is something in the Figure34 that I do not understand. You told me if&lt;/P&gt;&lt;P&gt;current is 10 mA, the pin output voltage/current is 4.9V/10mA. Does this&lt;/P&gt;&lt;P&gt;mean that if I want an output of 10 mA the Voh shall to be 4.9V? And if&lt;/P&gt;&lt;P&gt;that is so, how can I get 4.9V at the output with a voltage supply of 5V? I&lt;/P&gt;&lt;P&gt;thought that the Voh was set for all supplies, according to the Table 14:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/79874i55056A9343E1ACE9/image-size/large?v=v2&amp;amp;px=999" title="Screen Shot 2018-08-07 at 13.26.56.png" alt="Screen Shot 2018-08-07 at 13.26.56.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;On Thu, Aug 2, 2018 at 8:21 AM, xiangjun.rong &amp;lt;&lt;/SPAN&gt;&lt;A class="jive-link-email-small" href="mailto:admin@community.nxp.com"&gt;admin@community.nxp.com&lt;/A&gt;&lt;SPAN&gt;&amp;gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 07 Aug 2018 11:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798281#M1311</guid>
      <dc:creator>manuelcaracuel</dc:creator>
      <dc:date>2018-08-07T11:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum I/O source current per bit for the PCA9698?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798282#M1312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV class=""&gt;&lt;P&gt;Hi, Manuel,&lt;/P&gt;This is my understanding of Fig34, the fig 34 is tested with VDD 5V, the curve means that X coordinator VDD-VOH increase with the Y coordinator source current. For the +25 degree curve,&lt;/DIV&gt;&lt;DIV class=""&gt;I&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VDD-VOH&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VDD&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; VOH&lt;/DIV&gt;&lt;DIV class=""&gt;0mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5V&lt;/DIV&gt;&lt;DIV class=""&gt;8mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.1V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.9V&lt;/DIV&gt;&lt;DIV class=""&gt;15mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.2V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.8V&lt;/DIV&gt;&lt;DIV class=""&gt;20mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.3V &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 5V &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; 4.7V&lt;/DIV&gt;&lt;DIV class=""&gt;26mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.4V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.6V&lt;/DIV&gt;&lt;DIV class=""&gt;40mA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.6V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5V&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 4.4V&lt;/DIV&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;DIV class=""&gt;Hope it can help you&lt;/DIV&gt;&lt;DIV class=""&gt;BR&lt;/DIV&gt;&lt;DIV class=""&gt;Xiangjun Rong&lt;/DIV&gt;&lt;P&gt;&lt;/P&gt;&lt;DIV class=""&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 09:32:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798282#M1312</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-08-10T09:32:01Z</dc:date>
    </item>
    <item>
      <title>Re: What is the maximum I/O source current per bit for the PCA9698?</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798283#M1313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes I think that you are right. Thank you very much for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Manuel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Fri, Aug 10, 2018 at 11:32 AM, xiangjun.rong &amp;lt;admin@community.nxp.com&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Aug 2018 10:10:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/What-is-the-maximum-I-O-source-current-per-bit-for-the-PCA9698/m-p/798283#M1313</guid>
      <dc:creator>manuelcaracuel</dc:creator>
      <dc:date>2018-08-10T10:10:28Z</dc:date>
    </item>
  </channel>
</rss>