<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic SGTL5000 - VDDD in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-VDDD/m-p/794802#M1302</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we use the SGTL5000 in an i.MX6 system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem:&lt;/P&gt;&lt;P&gt;The VDDD voltage is higher than expected. The codec ist supplied by a MMPF0100-PMIC, a 1.2V-LDO is used. The Codec is the only load on 1.2V - aside from&amp;nbsp; some capacitors, there are no other parts. In the system, the voltage in the 1.2V-rail rises to 1.6V.&lt;/P&gt;&lt;P&gt;Suspected reason: The 3.3V-supply starts bevore the VDDD is suppliedm, so the SGTL5000 starts an internal regulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the SGTL5000 have an internal voltage regulator (as indicated in the datasheet)?&lt;/P&gt;&lt;P&gt;How does the SGTL5000 determine, if an external VDDD is supplied?&lt;/P&gt;&lt;P&gt;Are there any restricitions, on which sequence the supply voltages has to be applied?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot find any information about this in the datasheet. Thanks for any hep in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 25 Sep 2018 11:44:21 GMT</pubDate>
    <dc:creator>max123</dc:creator>
    <dc:date>2018-09-25T11:44:21Z</dc:date>
    <item>
      <title>SGTL5000 - VDDD</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-VDDD/m-p/794802#M1302</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;we use the SGTL5000 in an i.MX6 system.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Problem:&lt;/P&gt;&lt;P&gt;The VDDD voltage is higher than expected. The codec ist supplied by a MMPF0100-PMIC, a 1.2V-LDO is used. The Codec is the only load on 1.2V - aside from&amp;nbsp; some capacitors, there are no other parts. In the system, the voltage in the 1.2V-rail rises to 1.6V.&lt;/P&gt;&lt;P&gt;Suspected reason: The 3.3V-supply starts bevore the VDDD is suppliedm, so the SGTL5000 starts an internal regulator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does the SGTL5000 have an internal voltage regulator (as indicated in the datasheet)?&lt;/P&gt;&lt;P&gt;How does the SGTL5000 determine, if an external VDDD is supplied?&lt;/P&gt;&lt;P&gt;Are there any restricitions, on which sequence the supply voltages has to be applied?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I cannot find any information about this in the datasheet. Thanks for any hep in advance!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 25 Sep 2018 11:44:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SGTL5000-VDDD/m-p/794802#M1302</guid>
      <dc:creator>max123</dc:creator>
      <dc:date>2018-09-25T11:44:21Z</dc:date>
    </item>
  </channel>
</rss>