<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: MC56F8037 Pointer to Program Memory</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8037-Pointer-to-Program-Memory/m-p/759516#M1224</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;As you know that the flash must be erased, then programmed, any flash erasing, programming operation must follow up flash instruction, in DSC, flash is a peripheral.&lt;/P&gt;&lt;P&gt;You have to develop code based on PE(processor expert) in CodeWarrior for DSP56800E tools, the flash bean in PE provides the init, erasing programming api function&amp;nbsp; for the flash operation.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Jan 2018 06:12:02 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2018-01-30T06:12:02Z</dc:date>
    <item>
      <title>MC56F8037 Pointer to Program Memory</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8037-Pointer-to-Program-Memory/m-p/759515#M1223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I create a pointer to program flash?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is not working:&amp;nbsp;&amp;nbsp;uint16 *flash_ptr = (uint16*)0x7F30;&amp;nbsp; It looks like the data in View Memory when Page: x is selected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Jan 2018 19:49:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8037-Pointer-to-Program-Memory/m-p/759515#M1223</guid>
      <dc:creator>Mike_d</dc:creator>
      <dc:date>2018-01-25T19:49:33Z</dc:date>
    </item>
    <item>
      <title>Re: MC56F8037 Pointer to Program Memory</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8037-Pointer-to-Program-Memory/m-p/759516#M1224</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;As you know that the flash must be erased, then programmed, any flash erasing, programming operation must follow up flash instruction, in DSC, flash is a peripheral.&lt;/P&gt;&lt;P&gt;You have to develop code based on PE(processor expert) in CodeWarrior for DSP56800E tools, the flash bean in PE provides the init, erasing programming api function&amp;nbsp; for the flash operation.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Jan 2018 06:12:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/MC56F8037-Pointer-to-Program-Memory/m-p/759516#M1224</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-01-30T06:12:02Z</dc:date>
    </item>
  </channel>
</rss>