<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックSIM_RSTSTS is 0x0000</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SIM-RSTSTS-is-0x0000/m-p/734706#M1167</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to track down a reset issue on a 56F8345. At first the&amp;nbsp;SIM_RSTSTS register would show a COP reset but I can never hit a breakpoint in the COP isr.&amp;nbsp; After disabling the COP it continues to reset and now the&amp;nbsp;SIM_RSTSTS is 0x0000 after a reset.&amp;nbsp; What could cause this kind of behavior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Mar 2018 17:22:52 GMT</pubDate>
    <dc:creator>Mike_d</dc:creator>
    <dc:date>2018-03-06T17:22:52Z</dc:date>
    <item>
      <title>SIM_RSTSTS is 0x0000</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SIM-RSTSTS-is-0x0000/m-p/734706#M1167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to track down a reset issue on a 56F8345. At first the&amp;nbsp;SIM_RSTSTS register would show a COP reset but I can never hit a breakpoint in the COP isr.&amp;nbsp; After disabling the COP it continues to reset and now the&amp;nbsp;SIM_RSTSTS is 0x0000 after a reset.&amp;nbsp; What could cause this kind of behavior?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;-Mike&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Mar 2018 17:22:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SIM-RSTSTS-is-0x0000/m-p/734706#M1167</guid>
      <dc:creator>Mike_d</dc:creator>
      <dc:date>2018-03-06T17:22:52Z</dc:date>
    </item>
    <item>
      <title>Re: SIM_RSTSTS is 0x0000</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SIM-RSTSTS-is-0x0000/m-p/734707#M1168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Mike,&lt;/P&gt;&lt;P&gt;The COP module can not generate interrupt, it can only generate COP Reset.&amp;nbsp; you can not hit break point even if you set break point at the P:0x0002, it is debugger problem, that&amp;nbsp; is way you can not hit interrupt if you setting break point at P:0x0002. You can not hit interrupt if you set break point at interrupt vector table.&lt;/P&gt;&lt;P&gt;If the SIM_RSTSTS is 0x0000 , it means that Reset event does not happen.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Mar 2018 09:09:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SIM-RSTSTS-is-0x0000/m-p/734707#M1168</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2018-03-09T09:09:13Z</dc:date>
    </item>
    <item>
      <title>Re: SIM_RSTSTS is 0x0000</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/SIM-RSTSTS-is-0x0000/m-p/734708#M1169</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a similar problem. Often our application based on 56F8345 resets and we find in the registry SIM_RSTSTS 0x0000.&lt;BR /&gt;I wanted to ask you if you're using the CANbus module? Because I have doubts that it may be the cause.&lt;BR /&gt;I also wanted to ask you if you have the watch dog enabled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marco&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Mar 2018 11:52:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/SIM-RSTSTS-is-0x0000/m-p/734708#M1169</guid>
      <dc:creator>marco76</dc:creator>
      <dc:date>2018-03-23T11:52:01Z</dc:date>
    </item>
  </channel>
</rss>