<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックEMBC on 56724 is non-functional</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/EMBC-on-56724-is-non-functional/m-p/720685#M1148</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone successfully used the EMBC (External Memory Burst Controller) on a DSP56724 (or similar) ? I cannot get it to read or write at all reliably with sdram. Without it, sdram is so slow that it is unuseable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Dec 2017 18:04:07 GMT</pubDate>
    <dc:creator>nicholasrose</dc:creator>
    <dc:date>2017-12-13T18:04:07Z</dc:date>
    <item>
      <title>EMBC on 56724 is non-functional</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/EMBC-on-56724-is-non-functional/m-p/720685#M1148</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has anyone successfully used the EMBC (External Memory Burst Controller) on a DSP56724 (or similar) ? I cannot get it to read or write at all reliably with sdram. Without it, sdram is so slow that it is unuseable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Dec 2017 18:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/EMBC-on-56724-is-non-functional/m-p/720685#M1148</guid>
      <dc:creator>nicholasrose</dc:creator>
      <dc:date>2017-12-13T18:04:07Z</dc:date>
    </item>
  </channel>
</rss>