<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: Fault Filter in eflexPWM</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Fault-Filter-in-eflexPWM/m-p/714594#M1135</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This phenomenon is quite reasonable. The fault filter works in a way like this: there's an internal high frequency clock F_filt for detecting the input voltage level, say if the input voltage stays one&amp;nbsp;within continuous N periods of F_filt, the input is deemed to be one. For instance, suppose the input voltage is examined at each rising edge of F_filt, and N is set to 3, now see the attached pictures, the red waveform is the input signal on fault pin, and the blue one is F_filt. Both situation 1 and 2 can pass the filter, there's an error of +/- one period of F_filt.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="fault_filter.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42315i1F8E2BB0946966BF/image-size/large?v=v2&amp;amp;px=999" role="button" title="fault_filter.png" alt="fault_filter.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the case of 8036, F_filt is 96MHz/19 = 5.05MHz, so the period of F_filt is about 0.2us, which applies to your case.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 27 Sep 2017 02:50:04 GMT</pubDate>
    <dc:creator>sutter_zhou</dc:creator>
    <dc:date>2017-09-27T02:50:04Z</dc:date>
    <item>
      <title>Fault Filter in eflexPWM</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Fault-Filter-in-eflexPWM/m-p/714593#M1134</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;This is about Fault Filter in eflexPWM. Based on MC56F8036 where IPBus clock is 96MHz, PWMA_FFILTn is configured as 0x713 so filter time should be (7+3)*19/96=1.98us. But FFLAG is still set as 1 when input fault pin with a square wave&amp;nbsp;and the width is 1.8us. Is is normal or something wrong?&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/sutter"&gt;sutter&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 02:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Fault-Filter-in-eflexPWM/m-p/714593#M1134</guid>
      <dc:creator>chaozhuang-b500</dc:creator>
      <dc:date>2017-09-27T02:27:16Z</dc:date>
    </item>
    <item>
      <title>Re: Fault Filter in eflexPWM</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Fault-Filter-in-eflexPWM/m-p/714594#M1135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This phenomenon is quite reasonable. The fault filter works in a way like this: there's an internal high frequency clock F_filt for detecting the input voltage level, say if the input voltage stays one&amp;nbsp;within continuous N periods of F_filt, the input is deemed to be one. For instance, suppose the input voltage is examined at each rising edge of F_filt, and N is set to 3, now see the attached pictures, the red waveform is the input signal on fault pin, and the blue one is F_filt. Both situation 1 and 2 can pass the filter, there's an error of +/- one period of F_filt.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="fault_filter.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42315i1F8E2BB0946966BF/image-size/large?v=v2&amp;amp;px=999" role="button" title="fault_filter.png" alt="fault_filter.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;In the case of 8036, F_filt is 96MHz/19 = 5.05MHz, so the period of F_filt is about 0.2us, which applies to your case.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Sep 2017 02:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Fault-Filter-in-eflexPWM/m-p/714594#M1135</guid>
      <dc:creator>sutter_zhou</dc:creator>
      <dc:date>2017-09-27T02:50:04Z</dc:date>
    </item>
  </channel>
</rss>