<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal ControllersのトピックRe: Nuttx Running on FDRM K22</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Nuttx-Running-on-FDRM-K22/m-p/712243#M1132</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just have a look at the website of NuttX,&lt;A class="link-titled" href="http://nuttx.org/" title="http://nuttx.org/"&gt;NuttX Real-Time Operating System - NuttX Real-Time Operating System&lt;/A&gt;, and it is mentioned that Kinetis K20/K40/60/64/66 is supported. Actually I am not quite sure if thee K22 supported. You should check NuttX directly. Yes, the K20 and K22 really has a lot difference K20 is the first generation MCU and K22 is the next-generation MCU. The registers in these two generation MCU is not same. So you need to check with NuttX to know if it supported or not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Sep 2017 08:43:17 GMT</pubDate>
    <dc:creator>miduo</dc:creator>
    <dc:date>2017-09-28T08:43:17Z</dc:date>
    <item>
      <title>Nuttx Running on FDRM K22</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Nuttx-Running-on-FDRM-K22/m-p/712242#M1131</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The nuttx official software package includes the configuration for FDRM K64, K66 ,KL25,26 .&amp;nbsp;&amp;nbsp; So which configuration information can be used for KF22 as the mcu on the KF22 has a different footprint as on K64,K66 .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could anyone give me any instructions how to configure FDRM F22 on Nuttx?&lt;/P&gt;&lt;P&gt;Thanks a lot.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Sep 2017 06:45:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Nuttx-Running-on-FDRM-K22/m-p/712242#M1131</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2017-09-25T06:45:40Z</dc:date>
    </item>
    <item>
      <title>Re: Nuttx Running on FDRM K22</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Nuttx-Running-on-FDRM-K22/m-p/712243#M1132</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just have a look at the website of NuttX,&lt;A class="link-titled" href="http://nuttx.org/" title="http://nuttx.org/"&gt;NuttX Real-Time Operating System - NuttX Real-Time Operating System&lt;/A&gt;, and it is mentioned that Kinetis K20/K40/60/64/66 is supported. Actually I am not quite sure if thee K22 supported. You should check NuttX directly. Yes, the K20 and K22 really has a lot difference K20 is the first generation MCU and K22 is the next-generation MCU. The registers in these two generation MCU is not same. So you need to check with NuttX to know if it supported or not.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Sep 2017 08:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Nuttx-Running-on-FDRM-K22/m-p/712243#M1132</guid>
      <dc:creator>miduo</dc:creator>
      <dc:date>2017-09-28T08:43:17Z</dc:date>
    </item>
    <item>
      <title>Re: Nuttx Running on FDRM K22</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Nuttx-Running-on-FDRM-K22/m-p/712244#M1133</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;HI , Fang Li&lt;/DIV&gt;&lt;DIV&gt;Thanks.&lt;/DIV&gt;&lt;DIV&gt;When I put nuttx.bin file to MBED USB&amp;nbsp; folder, it&amp;nbsp; disconnected suddenly , and reconnected after a while. So did in the bootloader folder, when updating the bootloader firmware.&lt;/DIV&gt;&lt;DIV&gt;Do you have a solution for such kind of issues.&amp;nbsp;&amp;nbsp; &lt;/DIV&gt;&lt;DIV&gt;Another question is that when i put a .bin file into this MBED folder , will it be loaded into ARM flash immeditately or after pressing the reset button?&lt;/DIV&gt;&lt;DIV&gt;I use OpenSDA 2.1 and &lt;SPAN class=""&gt;CMSIS-DAP&lt;/SPAN&gt; MBED in a linux environment.&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 01:48:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Nuttx-Running-on-FDRM-K22/m-p/712244#M1133</guid>
      <dc:creator>alvenwu</dc:creator>
      <dc:date>2017-10-12T01:48:50Z</dc:date>
    </item>
  </channel>
</rss>