<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: enumerate the USB host functionality in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/enumerate-the-USB-host-functionality/m-p/701637#M1107</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Kishor&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;it is impossible to use GPIO pins as USB host interface. On the MC56F8037 Demo board, there is a USB-uart bridge IC called CP2102, but the CP2102 can be only a device rather than a host.&lt;BR /&gt;you can use the kinetis family with on-chip USB module as USB host, and MC56F8037 can communicate with the Kinmetis via spi, uart...&lt;BR /&gt;BTW, you can use the Kinetis family with USB module/PWM/ADC/timer modules to develop UPS.&lt;BR /&gt;For kinetis, we have developed the usb stack for both host/device.&lt;BR /&gt;Hope it can help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;Xiangjun Rong&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Aug 2017 07:29:34 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2017-08-23T07:29:34Z</dc:date>
    <item>
      <title>enumerate the USB host functionality</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/enumerate-the-USB-host-functionality/m-p/701636#M1106</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hai, all,&lt;/P&gt;&lt;P&gt;some times you feel i am asking some thing strange,But i am tied with a problem associated with the subject.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Is there any possibility to &lt;STRONG&gt;enumerate&lt;/STRONG&gt; the &lt;STRONG&gt;USB host functionality&lt;/STRONG&gt; inside a processor &lt;STRONG&gt;with out USB peripheral&lt;/STRONG&gt;. If so please give some open source example/ &lt;SPAN style="text-decoration: underline;"&gt;USB stack&lt;/SPAN&gt; / Third party stack (for other device) with the HOST ability. My micro controller is &lt;STRONG style="font-family: trebuchet ms,geneva,sans-serif;"&gt;MC56F8037.&lt;/STRONG&gt; Any updates or hinds in above subject is a great help for me!!!!!.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Aug 2017 08:12:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/enumerate-the-USB-host-functionality/m-p/701636#M1106</guid>
      <dc:creator>kishorravi</dc:creator>
      <dc:date>2017-08-18T08:12:31Z</dc:date>
    </item>
    <item>
      <title>Re: enumerate the USB host functionality</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/enumerate-the-USB-host-functionality/m-p/701637#M1107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Kishor&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;it is impossible to use GPIO pins as USB host interface. On the MC56F8037 Demo board, there is a USB-uart bridge IC called CP2102, but the CP2102 can be only a device rather than a host.&lt;BR /&gt;you can use the kinetis family with on-chip USB module as USB host, and MC56F8037 can communicate with the Kinmetis via spi, uart...&lt;BR /&gt;BTW, you can use the Kinetis family with USB module/PWM/ADC/timer modules to develop UPS.&lt;BR /&gt;For kinetis, we have developed the usb stack for both host/device.&lt;BR /&gt;Hope it can help you.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;BR&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: Arial;"&gt;Xiangjun Rong&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 07:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/enumerate-the-USB-host-functionality/m-p/701637#M1107</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2017-08-23T07:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: enumerate the USB host functionality</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/enumerate-the-USB-host-functionality/m-p/701638#M1108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;SPAN class=""&gt;&lt;A _jive_internal="true" data-content-finding="Community" data-userid="19420" data-username="xiangjun.rong" href="https://community.nxp.com/people/xiangjun.rong"&gt;Xiangjun.rong&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I also go through some researches and i also reach the same point.We are planning for scaling up of the processor.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you for your help. &lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/message/ece.kishor@gmial.com"&gt;Kishor R&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Aug 2017 08:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/enumerate-the-USB-host-functionality/m-p/701638#M1108</guid>
      <dc:creator>kishorravi</dc:creator>
      <dc:date>2017-08-23T08:27:47Z</dc:date>
    </item>
  </channel>
</rss>