<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Digital Signal Controllers中的主题 Debugger errors - Multilink FX</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Debugger-errors-Multilink-FX/m-p/692567#M1090</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a Multilink FX to connect to an MC56F8345.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've verified the debugger is ok by connecting to a 56F84789, and also managed to connect to the 8345 previously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when I try to connect to the target (56F8345) for a debug session, I get the following error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21939i9BAEEC0707F7C0E9/image-size/large?v=v2&amp;amp;px=999" title="Multilink_Error.jpg" alt="Multilink_Error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have tried the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* Multiple speeds (slowest, fastest, and others. Default is (24). )&lt;/P&gt;&lt;P&gt;* Creating a base example project for the 8345 using USB Tap and also separate project for Multilink FX&lt;/P&gt;&lt;P&gt;* Updating Multilink software&lt;/P&gt;&lt;P&gt;* Deleting the .metadata folder in the workspace and re-importing the CW10.6 project.&lt;/P&gt;&lt;P&gt;* Deleting the debug configuration and specifying a new one&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;None of the above has worked. I could connect into the target hardware last night, but have now lost that ability&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions welcome...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 May 2017 14:43:04 GMT</pubDate>
    <dc:creator>TurboMan</dc:creator>
    <dc:date>2017-05-24T14:43:04Z</dc:date>
    <item>
      <title>Debugger errors - Multilink FX</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Debugger-errors-Multilink-FX/m-p/692567#M1090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a Multilink FX to connect to an MC56F8345.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've verified the debugger is ok by connecting to a 56F84789, and also managed to connect to the 8345 previously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now when I try to connect to the target (56F8345) for a debug session, I get the following error:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/21939i9BAEEC0707F7C0E9/image-size/large?v=v2&amp;amp;px=999" title="Multilink_Error.jpg" alt="Multilink_Error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I have tried the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* Multiple speeds (slowest, fastest, and others. Default is (24). )&lt;/P&gt;&lt;P&gt;* Creating a base example project for the 8345 using USB Tap and also separate project for Multilink FX&lt;/P&gt;&lt;P&gt;* Updating Multilink software&lt;/P&gt;&lt;P&gt;* Deleting the .metadata folder in the workspace and re-importing the CW10.6 project.&lt;/P&gt;&lt;P&gt;* Deleting the debug configuration and specifying a new one&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;None of the above has worked. I could connect into the target hardware last night, but have now lost that ability&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestions welcome...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2017 14:43:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Debugger-errors-Multilink-FX/m-p/692567#M1090</guid>
      <dc:creator>TurboMan</dc:creator>
      <dc:date>2017-05-24T14:43:04Z</dc:date>
    </item>
    <item>
      <title>Re: Debugger errors - Multilink FX</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/Debugger-errors-Multilink-FX/m-p/692568#M1091</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;False alarm...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found a solder whisker shorting out a clock pin / pin near the clock input. Debugger working correctly now...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2017 15:31:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/Debugger-errors-Multilink-FX/m-p/692568#M1091</guid>
      <dc:creator>TurboMan</dc:creator>
      <dc:date>2017-05-24T15:31:51Z</dc:date>
    </item>
  </channel>
</rss>