<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PTN3363 TMDS input voltage level in Digital Signal Controllers</title>
    <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN3363-TMDS-input-voltage-level/m-p/681458#M1054</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm developing an application in which an HDMI signal needs to be shifted up from 1.8V to 3.3V. At page 18 of &lt;A href="http://www.nxp.com/documents/data_sheet/PTN3363.pdf"&gt;this&lt;/A&gt; document characteristics of PTN3363 are shown: could someone please confirm me that V_RX and V_RX_Diff level range will accept my HDMI input? I'm a bit afraid of what's said on the datasheet "PTN3363 operates only when the input signal level is above certain minimum threshold (as per VRX_DIFFp-p). If the input falls below that minimum threshold, the outputs are squelched."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Matteo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 09 Jun 2017 07:59:00 GMT</pubDate>
    <dc:creator>matteoconti</dc:creator>
    <dc:date>2017-06-09T07:59:00Z</dc:date>
    <item>
      <title>PTN3363 TMDS input voltage level</title>
      <link>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN3363-TMDS-input-voltage-level/m-p/681458#M1054</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm developing an application in which an HDMI signal needs to be shifted up from 1.8V to 3.3V. At page 18 of &lt;A href="http://www.nxp.com/documents/data_sheet/PTN3363.pdf"&gt;this&lt;/A&gt; document characteristics of PTN3363 are shown: could someone please confirm me that V_RX and V_RX_Diff level range will accept my HDMI input? I'm a bit afraid of what's said on the datasheet "PTN3363 operates only when the input signal level is above certain minimum threshold (as per VRX_DIFFp-p). If the input falls below that minimum threshold, the outputs are squelched."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Matteo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Jun 2017 07:59:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Digital-Signal-Controllers/PTN3363-TMDS-input-voltage-level/m-p/681458#M1054</guid>
      <dc:creator>matteoconti</dc:creator>
      <dc:date>2017-06-09T07:59:00Z</dc:date>
    </item>
  </channel>
</rss>