<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Drones and Rovers中的主题 Propeller size</title>
    <link>https://community.nxp.com/t5/Drones-and-Rovers/Propeller-size/m-p/1576177#M64</link>
    <description>&lt;P&gt;Can anyone, please tell what is the size of the propeller given with the kit?&lt;/P&gt;</description>
    <pubDate>Mon, 02 Jan 2023 19:33:01 GMT</pubDate>
    <dc:creator>Shake21</dc:creator>
    <dc:date>2023-01-02T19:33:01Z</dc:date>
    <item>
      <title>Propeller size</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/Propeller-size/m-p/1576177#M64</link>
      <description>&lt;P&gt;Can anyone, please tell what is the size of the propeller given with the kit?&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 19:33:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/Propeller-size/m-p/1576177#M64</guid>
      <dc:creator>Shake21</dc:creator>
      <dc:date>2023-01-02T19:33:01Z</dc:date>
    </item>
    <item>
      <title>Re: Propeller size</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/Propeller-size/m-p/1576193#M65</link>
      <description>&lt;P&gt;Hi Shake21, if i'm not mistaken there are two sets included. 11" and 12". I would recommend using just the 12" ones that are stifter and have better performance. If there is just one size it's for sure the 12".&lt;/P&gt;</description>
      <pubDate>Mon, 02 Jan 2023 20:32:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/Propeller-size/m-p/1576193#M65</guid>
      <dc:creator>GeraldP</dc:creator>
      <dc:date>2023-01-02T20:32:07Z</dc:date>
    </item>
  </channel>
</rss>