<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Drones and RoversのトピックRe: one UWB anchor with many tags</title>
    <link>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485091#M43</link>
    <description>&lt;P&gt;Hi Roman,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are using Time difference of Arrival(TDOA) then multiple anchors can do ranging and AoA with hundreds of Tags simultaneously.&lt;/P&gt;
&lt;P&gt;If you are using Two way double-sided ranging (TW-DSR) then the NXP Trimension SR150 allows for 5 ranging sessions with a maximum of 12 devices. (Distance and AoA)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope that answers your question.&lt;/P&gt;</description>
    <pubDate>Wed, 06 Jul 2022 05:55:14 GMT</pubDate>
    <dc:creator>Low_Orbit</dc:creator>
    <dc:date>2022-07-06T05:55:14Z</dc:date>
    <item>
      <title>one UWB anchor with many tags</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1484679#M42</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;Can one UWB anchor detect range and AOA of many tags simultaneously?&lt;/P&gt;&lt;P&gt;If so , how many tags one anchor can support? In what rate?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank You&amp;nbsp;&lt;/P&gt;&lt;P&gt;Roman&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jul 2022 13:16:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1484679#M42</guid>
      <dc:creator>RG30</dc:creator>
      <dc:date>2022-07-05T13:16:42Z</dc:date>
    </item>
    <item>
      <title>Re: one UWB anchor with many tags</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485091#M43</link>
      <description>&lt;P&gt;Hi Roman,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you are using Time difference of Arrival(TDOA) then multiple anchors can do ranging and AoA with hundreds of Tags simultaneously.&lt;/P&gt;
&lt;P&gt;If you are using Two way double-sided ranging (TW-DSR) then the NXP Trimension SR150 allows for 5 ranging sessions with a maximum of 12 devices. (Distance and AoA)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I hope that answers your question.&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 05:55:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485091#M43</guid>
      <dc:creator>Low_Orbit</dc:creator>
      <dc:date>2022-07-06T05:55:14Z</dc:date>
    </item>
    <item>
      <title>Re: one UWB anchor with many tags</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485166#M44</link>
      <description>&lt;P&gt;"&lt;SPAN&gt;If you are using Two way double-sided ranging (TW-DSR) then the NXP Trimension SR150 allows for 5 ranging sessions with a maximum of 12 devices. (Distance and AoA)"&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;thank you for the answers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm interested in the TW-DSR ranging and AoA&lt;/P&gt;&lt;P&gt;Can you please clarify, when you say "5 ranging sessions" you mean 5HZ of sampling rate of one anchor or 5 anchors working in proximity?&lt;/P&gt;&lt;P&gt;When you say 12 devices , you mean 12 tags with one anchor?&lt;/P&gt;&lt;P&gt;1.I'm trying to understand how many tags one anchor can work with ?&lt;/P&gt;&lt;P&gt;2.How many&amp;nbsp; anchors one tag can work with?&lt;/P&gt;&lt;P&gt;3. Is there a interference between anchors that work close to each other?&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 07:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485166#M44</guid>
      <dc:creator>RG30</dc:creator>
      <dc:date>2022-07-06T07:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: one UWB anchor with many tags</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485208#M45</link>
      <description>&lt;P&gt;Hello Roman,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;A Ranging &lt;STRONG&gt;session&lt;/STRONG&gt; is a configured ranging sequence with up to 12 partner devices. In total 13 devices can take part in one session. The &lt;STRONG&gt;session&lt;/STRONG&gt; executes a ranging &lt;STRONG&gt;sequence&lt;/STRONG&gt;, consisting of multiple ranging messages dependent on ranging mode.&lt;/P&gt;&lt;P&gt;The ranging rate is limited by the number of messages in the ranging &lt;STRONG&gt;sequence&lt;/STRONG&gt;. Using TW-DSR we can achieve above 40 Hertz with 5 devices (4 Tags and 1 Anchor). More message = Lower Rate&lt;/P&gt;&lt;P&gt;The NXP Trimension SR150/SR040 supports 5 active sessions.&lt;/P&gt;&lt;P&gt;1. In theory an UWB device can range with 12x5 (=60) devices (Tags and other Anchors)&lt;/P&gt;&lt;P&gt;2. Anchors and Tags differ only in naming and purpose, the UWB chip is identical (either SR040 or SR150).&lt;/P&gt;&lt;P&gt;3. yes if they Range at the same time, then interference might be an issue. This can be mitigated by using multiple channels (5, 6, 8, 9).&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jul 2022 08:31:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485208#M45</guid>
      <dc:creator>Low_Orbit</dc:creator>
      <dc:date>2022-07-06T08:31:04Z</dc:date>
    </item>
    <item>
      <title>Re: one UWB anchor with many tags</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485969#M46</link>
      <description>&lt;P&gt;ok , thank you&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 07 Jul 2022 06:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1485969#M46</guid>
      <dc:creator>RG30</dc:creator>
      <dc:date>2022-07-07T06:36:20Z</dc:date>
    </item>
    <item>
      <title>Re: one UWB anchor with many tags</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1528172#M50</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/179951"&gt;@Low_Orbit&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;Thanks for your response very helpful from my side.&amp;nbsp;&lt;BR /&gt;I do have the SR150/SR040 for experiments (academic purposes) I am stuck on how to use new smart devices with in-built UWB functionalities as tags: My goal is to have multiple users but I only have 2 tags that came with the kit.&lt;/P&gt;&lt;P&gt;How do I go by this..?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Sep 2022 13:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/one-UWB-anchor-with-many-tags/m-p/1528172#M50</guid>
      <dc:creator>Goodlet</dc:creator>
      <dc:date>2022-09-26T13:34:08Z</dc:date>
    </item>
  </channel>
</rss>