<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Drones and Rovers中的主题 RDDRONE-BMS772 I2C crashes after a while</title>
    <link>https://community.nxp.com/t5/Drones-and-Rovers/RDDRONE-BMS772-I2C-crashes-after-a-while/m-p/1423536#M38</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'm using the SMBUS implementation to retrieve values from the RDDRONE-BMS772 (FW bms5.0-10.1).&lt;BR /&gt;After a random time (usually more then 20 minutes) the I2C-communicaiton crashes until I reboot the BMS from CLI.&lt;BR /&gt;&lt;BR /&gt;I use a simple pyhton script on NVIDIA Xavier NX dev-kit using "smbus2 0.4.1".&lt;BR /&gt;The devkit has &lt;SPAN class=""&gt;&lt;SPAN&gt;2.2KΩ pull-ups integrated and the BMS is the only slave on the I2C_2.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Rebooting the Xavier doesn't help but rebooting the BMS works. So I think the problem is on the BMS side. As I'm not familiar with the BMS and nuttx yet I need some help getting started for debuging here.&lt;/P&gt;</description>
    <pubDate>Sun, 06 Mar 2022 16:41:22 GMT</pubDate>
    <dc:creator>thetruthishere</dc:creator>
    <dc:date>2022-03-06T16:41:22Z</dc:date>
    <item>
      <title>RDDRONE-BMS772 I2C crashes after a while</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/RDDRONE-BMS772-I2C-crashes-after-a-while/m-p/1423536#M38</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I'm using the SMBUS implementation to retrieve values from the RDDRONE-BMS772 (FW bms5.0-10.1).&lt;BR /&gt;After a random time (usually more then 20 minutes) the I2C-communicaiton crashes until I reboot the BMS from CLI.&lt;BR /&gt;&lt;BR /&gt;I use a simple pyhton script on NVIDIA Xavier NX dev-kit using "smbus2 0.4.1".&lt;BR /&gt;The devkit has &lt;SPAN class=""&gt;&lt;SPAN&gt;2.2KΩ pull-ups integrated and the BMS is the only slave on the I2C_2.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Rebooting the Xavier doesn't help but rebooting the BMS works. So I think the problem is on the BMS side. As I'm not familiar with the BMS and nuttx yet I need some help getting started for debuging here.&lt;/P&gt;</description>
      <pubDate>Sun, 06 Mar 2022 16:41:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/RDDRONE-BMS772-I2C-crashes-after-a-while/m-p/1423536#M38</guid>
      <dc:creator>thetruthishere</dc:creator>
      <dc:date>2022-03-06T16:41:22Z</dc:date>
    </item>
  </channel>
</rss>