<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Drones and RoversのトピックRe: Motor calibrations</title>
    <link>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1299080#M26</link>
    <description>&lt;P&gt;Ok. Sorry about the motor problem. You can get a replacement from NXP. I'll send you a private email&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Mon, 28 Jun 2021 12:04:14 GMT</pubDate>
    <dc:creator>iaingalloway</dc:creator>
    <dc:date>2021-06-28T12:04:14Z</dc:date>
    <item>
      <title>Motor calibrations</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1298698#M23</link>
      <description>&lt;P&gt;Hi, i bought the HGDRONEK66 and all connection and assembly i followed through the gitbook, but out of the four motors, one doesnt rotate. i tried switching the esc with different motors, others work fine with it. so the motor is the problem. is there anyway to check if the motor is operable or it is just faulty as i received it? the motor just jitters when i tried calibrating it and doesnt spins. havent tried flying yet.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 27 Jun 2021 10:44:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1298698#M23</guid>
      <dc:creator>ArifKamal</dc:creator>
      <dc:date>2021-06-27T10:44:45Z</dc:date>
    </item>
    <item>
      <title>Re: Motor calibrations</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1298709#M24</link>
      <description>&lt;P&gt;My guess is that u are using M3 screws that are too long. It is mentioned in the instruction that the short M3 screws included need to be used. Otherwise there is a risc of shortening the coils on the motor. Please check that.&lt;/P&gt;&lt;P&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/15914"&gt;@iaingalloway&lt;/a&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 27 Jun 2021 17:22:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1298709#M24</guid>
      <dc:creator>dk7xe</dc:creator>
      <dc:date>2021-06-27T17:22:44Z</dc:date>
    </item>
    <item>
      <title>Re: Motor calibrations</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1298713#M25</link>
      <description>&lt;P&gt;Nope, im using the short screws like the ones suggested in the gitbook. I even tried calibrating the motor in question without the screws screwed in. It only jitters when i tried.&lt;/P&gt;</description>
      <pubDate>Sun, 27 Jun 2021 19:47:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1298713#M25</guid>
      <dc:creator>ArifKamal</dc:creator>
      <dc:date>2021-06-27T19:47:59Z</dc:date>
    </item>
    <item>
      <title>Re: Motor calibrations</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1299080#M26</link>
      <description>&lt;P&gt;Ok. Sorry about the motor problem. You can get a replacement from NXP. I'll send you a private email&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 12:04:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1299080#M26</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2021-06-28T12:04:14Z</dc:date>
    </item>
    <item>
      <title>Re: Motor calibrations</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1299082#M27</link>
      <description>&lt;P&gt;FWIW - jittering would suggest that only two of the three windings are connected. If you felt like it, you could measure resistance between each combination of two of the three wires.&lt;/P&gt;
&lt;P&gt;(But this is just for interest sake, no issue in replacing the motor from NXP side)&lt;/P&gt;</description>
      <pubDate>Mon, 28 Jun 2021 12:07:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/Motor-calibrations/m-p/1299082#M27</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2021-06-28T12:07:24Z</dc:date>
    </item>
  </channel>
</rss>