<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PWM Outputs on RDDRONE-FMUK66 in Drones and Rovers</title>
    <link>https://community.nxp.com/t5/Drones-and-Rovers/PWM-Outputs-on-RDDRONE-FMUK66/m-p/1224089#M10</link>
    <description>&lt;P&gt;&lt;SPAN&gt;How many PWM outputs does the RDDRONE FMUK66 hardware kit support ? I have a VTOL with 4 motors and 5 servos. Can this kit control up to 9 motors ?&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 01 Feb 2021 12:58:05 GMT</pubDate>
    <dc:creator>Kade98002</dc:creator>
    <dc:date>2021-02-01T12:58:05Z</dc:date>
    <item>
      <title>PWM Outputs on RDDRONE-FMUK66</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/PWM-Outputs-on-RDDRONE-FMUK66/m-p/1224089#M10</link>
      <description>&lt;P&gt;&lt;SPAN&gt;How many PWM outputs does the RDDRONE FMUK66 hardware kit support ? I have a VTOL with 4 motors and 5 servos. Can this kit control up to 9 motors ?&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 01 Feb 2021 12:58:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/PWM-Outputs-on-RDDRONE-FMUK66/m-p/1224089#M10</guid>
      <dc:creator>Kade98002</dc:creator>
      <dc:date>2021-02-01T12:58:05Z</dc:date>
    </item>
    <item>
      <title>Re: PWM Outputs on RDDRONE-FMUK66</title>
      <link>https://community.nxp.com/t5/Drones-and-Rovers/PWM-Outputs-on-RDDRONE-FMUK66/m-p/1231011#M13</link>
      <description>&lt;P&gt;RevD of the RDDRONE-FMUK66 has 6 PWM outputs.&lt;BR /&gt;RevE is in progress and it will have 8 PWM outputs.&lt;BR /&gt;&lt;BR /&gt;NOTE: &lt;BR /&gt;NXP UCANS32K146-01 is a UAVCANv1 Development board - it has two PWM outputs and also runs PX4 internally.&lt;BR /&gt;It could be used to add more PWM channels (and sensor inputs etc.)&lt;BR /&gt;UAVCANv1 is in its infancy, and as of today external PWM are not supported "turnkey" yet, but they will be.&lt;BR /&gt;Currently UAVCANv1 has a GPS example and a BMS example.&lt;/P&gt;</description>
      <pubDate>Mon, 15 Feb 2021 14:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Drones-and-Rovers/PWM-Outputs-on-RDDRONE-FMUK66/m-p/1231011#M13</guid>
      <dc:creator>iaingalloway</dc:creator>
      <dc:date>2021-02-15T14:11:31Z</dc:date>
    </item>
  </channel>
</rss>