<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: script executing without CCS starting in CodeWarrior for StarCore</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/script-executing-without-CCS-starting/m-p/267915#M429</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CCS represents the connection server used by the CodeWarrior to "talk" with the target (the MSC8156ADS board).&lt;/P&gt;&lt;P&gt;The TCL scripts design for Debugger Shell are not 100% compatible with the CCS TCL scripting, but basically you can reuse the CCS available commands to write a script to load and start a program on the target via the CCS without IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nonetheless, this is a complicated task, you will need to emulate the CW debugger behavior with CCS low level commands.&lt;/P&gt;&lt;P&gt;To see the list of available CCS commands, just open a CCS console and type "ccs::"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps &amp;amp; Good luck!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Jun 2013 14:17:21 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2013-06-04T14:17:21Z</dc:date>
    <item>
      <title>script executing without CCS starting</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/script-executing-without-CCS-starting/m-p/267914#M428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt; I want to load and start program for MSC8156ADS without starting CCS. Can i execute *.tcl-script(intended for Debugger S&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;hell originally) in windows command line without CCS starting?. Can i use debugger without IDE starting, just by comman line control?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Thank you.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 May 2013 14:11:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/script-executing-without-CCS-starting/m-p/267914#M428</guid>
      <dc:creator>s_kalop</dc:creator>
      <dc:date>2013-05-31T14:11:38Z</dc:date>
    </item>
    <item>
      <title>Re: script executing without CCS starting</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/script-executing-without-CCS-starting/m-p/267915#M429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CCS represents the connection server used by the CodeWarrior to "talk" with the target (the MSC8156ADS board).&lt;/P&gt;&lt;P&gt;The TCL scripts design for Debugger Shell are not 100% compatible with the CCS TCL scripting, but basically you can reuse the CCS available commands to write a script to load and start a program on the target via the CCS without IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Nonetheless, this is a complicated task, you will need to emulate the CW debugger behavior with CCS low level commands.&lt;/P&gt;&lt;P&gt;To see the list of available CCS commands, just open a CCS console and type "ccs::"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps &amp;amp; Good luck!&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Jun 2013 14:17:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/script-executing-without-CCS-starting/m-p/267915#M429</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2013-06-04T14:17:21Z</dc:date>
    </item>
    <item>
      <title>Re: script executing without CCS starting</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/script-executing-without-CCS-starting/m-p/267916#M430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for reply, Daniel! I recognized that it is impossible. But with TI Code Composer Studio such standalone debugging is possible, so i thought it is so for CW. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2013 19:55:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/script-executing-without-CCS-starting/m-p/267916#M430</guid>
      <dc:creator>s_kalop</dc:creator>
      <dc:date>2013-06-05T19:55:51Z</dc:date>
    </item>
  </channel>
</rss>