<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for StarCore中的主题 Re: Causing Virtual Interrupts from the Debugger?</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Causing-Virtual-Interrupts-from-the-Debugger/m-p/213782#M374</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Answering my own question here I have to say it works now. Just writing to the appropriate GIC register does the trick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2011 15:17:05 GMT</pubDate>
    <dc:creator>kiliant3072</dc:creator>
    <dc:date>2011-08-02T15:17:05Z</dc:date>
    <item>
      <title>Causing Virtual Interrupts from the Debugger?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Causing-Virtual-Interrupts-from-the-Debugger/m-p/213781#M373</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm wondering whether it is possible to generate a virtual interrupt by writing a value to the appropriate memory location on the 8156. I tried but it only works from inside the program when running on an ADS board and not from the debugger.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The goal is to use TCL to stimulate an interrupt i.e. through a change or mem command. This doesn't work and so I tried to pause the program and use the memory window to set the register in memory. An interrupt is not generated however.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you have any suggestions on how to cause an interrupt from the debugger I would be glad.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Kilian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Jun 2011 20:53:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Causing-Virtual-Interrupts-from-the-Debugger/m-p/213781#M373</guid>
      <dc:creator>kiliant3072</dc:creator>
      <dc:date>2011-06-09T20:53:06Z</dc:date>
    </item>
    <item>
      <title>Re: Causing Virtual Interrupts from the Debugger?</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Causing-Virtual-Interrupts-from-the-Debugger/m-p/213782#M374</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Answering my own question here I have to say it works now. Just writing to the appropriate GIC register does the trick.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Aug 2011 15:17:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Causing-Virtual-Interrupts-from-the-Debugger/m-p/213782#M374</guid>
      <dc:creator>kiliant3072</dc:creator>
      <dc:date>2011-08-02T15:17:05Z</dc:date>
    </item>
  </channel>
</rss>