<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for StarCore中的主题 Re: *.appli file with librarian</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/appli-file-with-librarian/m-p/172126#M36</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Nov 2012 08:38:58 GMT</pubDate>
    <dc:creator>s_kalop</dc:creator>
    <dc:date>2012-11-13T08:38:58Z</dc:date>
    <item>
      <title>*.appli file with librarian</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/appli-file-with-librarian/m-p/172124#M34</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;I have two projects for msc8156 in CW 10.2.1: simple library project and StarCore project using that library. Library has some large array of data which i want to place in DDR with help of *.appli file. I wrote this appli file for project, not a library, built both, but this fails and large array was placed in M2. So i wrote appli for library project, built it, than built main project without *.appli and array was successfully placed in DDR. I don't understand how it can be. I suppose that library project do not use linker and using *.appli file makes sense only for "application" project type. What is my fault? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Nov 2012 13:33:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/appli-file-with-librarian/m-p/172124#M34</guid>
      <dc:creator>s_kalop</dc:creator>
      <dc:date>2012-11-12T13:33:40Z</dc:date>
    </item>
    <item>
      <title>Re: *.appli file with librarian</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/appli-file-with-librarian/m-p/172125#M35</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In fact when you place an object in a user defined section inside of a .appli file, the assignment is performed at compilation time. &lt;/P&gt;&lt;P&gt;So if you intend to place a variable into DDR, you need to associate the .appli file to the project which is generating the library. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The section where the variable is allocated is stored in the.eln file generated by the compiler. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2012 07:56:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/appli-file-with-librarian/m-p/172125#M35</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2012-11-13T07:56:21Z</dc:date>
    </item>
    <item>
      <title>Re: *.appli file with librarian</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/appli-file-with-librarian/m-p/172126#M36</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Nov 2012 08:38:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/appli-file-with-librarian/m-p/172126#M36</guid>
      <dc:creator>s_kalop</dc:creator>
      <dc:date>2012-11-13T08:38:58Z</dc:date>
    </item>
  </channel>
</rss>