<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Memory browser vs mem command with Debugger Shell in CodeWarrior for StarCore</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Memory-browser-vs-mem-command-with-Debugger-Shell/m-p/168207#M31</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi klm78,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems to be indeed a cache related behavior. I'll check this and return with details as soon as I'll have access to a board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nonetheless, the preferred way of dumping memory are Target Tasks/Import-Export memory.&lt;/P&gt;&lt;P&gt;Also, please be aware that there are two types of Memory views supported in CW - one of them is the Memory Browser view with a reduce set of features and the other one is Memory view.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I advice you to use the Memory view, where you can place a monitor (for example at 0x40000000) and in the same time you can specify which type of memory is used (physical, virtual for data or virtual for program)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 22 Sep 2011 00:25:43 GMT</pubDate>
    <dc:creator>Daniel_Popa</dc:creator>
    <dc:date>2011-09-22T00:25:43Z</dc:date>
    <item>
      <title>Memory browser vs mem command with Debugger Shell</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Memory-browser-vs-mem-command-with-Debugger-Shell/m-p/168206#M30</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;We have some doubt concerning the memory browser window in CW 10.1.8 for StarCore.&lt;/P&gt;&lt;P&gt;Our Configuration is ADS8156&lt;/P&gt;&lt;P&gt;If we open this browser at a memory adress in DDR &amp;gt; 0x40000000 and look at the same adress &amp;nbsp;with Debugger Shell mem command&lt;/P&gt;&lt;P&gt;The result is the same.&lt;/P&gt;&lt;P&gt;If we modify &amp;nbsp;a value memory cell in the browser, there's no change observed with mem command in Debugger Shell&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Which way is the most accurate for dumping memory in Debug Mode ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is this issue could be due to CACHE management ?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;BR. klm78&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Sep 2011 23:22:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Memory-browser-vs-mem-command-with-Debugger-Shell/m-p/168206#M30</guid>
      <dc:creator>klm78</dc:creator>
      <dc:date>2011-09-20T23:22:03Z</dc:date>
    </item>
    <item>
      <title>Re: Memory browser vs mem command with Debugger Shell</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Memory-browser-vs-mem-command-with-Debugger-Shell/m-p/168207#M31</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi klm78,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Seems to be indeed a cache related behavior. I'll check this and return with details as soon as I'll have access to a board.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Nonetheless, the preferred way of dumping memory are Target Tasks/Import-Export memory.&lt;/P&gt;&lt;P&gt;Also, please be aware that there are two types of Memory views supported in CW - one of them is the Memory Browser view with a reduce set of features and the other one is Memory view.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I advice you to use the Memory view, where you can place a monitor (for example at 0x40000000) and in the same time you can specify which type of memory is used (physical, virtual for data or virtual for program)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Sep 2011 00:25:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Memory-browser-vs-mem-command-with-Debugger-Shell/m-p/168207#M31</guid>
      <dc:creator>Daniel_Popa</dc:creator>
      <dc:date>2011-09-22T00:25:43Z</dc:date>
    </item>
  </channel>
</rss>