<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problems with development board MSC8156ADS in CodeWarrior for StarCore</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Problems-with-development-board-MSC8156ADS/m-p/146331#M2</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We need to make sure that the USBTAP is set up correctly for debugging.&amp;nbsp; Follow steps below:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; Start--&amp;gt;Programs--&amp;gt;Freescale CodeWarrior --&amp;gt;CodeWarrior for StarCore --&amp;gt;CodeWarrior Connection Server.&amp;nbsp; The CodeWarrior Connection Server window appears in the system toolbar.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; Double-click on CodeWarrior Connection Server icon.&amp;nbsp; The CodeWarrior Connection Server window appears.&lt;/P&gt;&lt;P&gt;3.&amp;nbsp; Type show cc -- display the correctly configured device&lt;/P&gt;&lt;P&gt;4.&amp;nbsp; Type delete all -- delete configured devices.&lt;/P&gt;&lt;P&gt;5.&amp;nbsp; Type show cc -- display the correctly configured devices.&amp;nbsp; At this point it should say that there are no command converter configured.&lt;/P&gt;&lt;P&gt;6.&amp;nbsp; Type config cc utap&lt;/P&gt;&lt;P&gt;7.&amp;nbsp; Type show cc --&amp;gt;It should state that it is sending code to the USB TAP.&lt;/P&gt;&lt;P&gt;8.&amp;nbsp; Try to debug your application.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Jul 2011 22:07:31 GMT</pubDate>
    <dc:creator>Irene</dc:creator>
    <dc:date>2011-07-06T22:07:31Z</dc:date>
    <item>
      <title>Problems with development board MSC8156ADS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Problems-with-development-board-MSC8156ADS/m-p/146330#M1</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello!&lt;/P&gt;&lt;P&gt;I have some problems with development board MSC8156ADS. For undefined reasons processor could not be upload via USB with a help of CodeWarrior SC. I’ve never met such situation before. Also CodeWarrior error message appears on the screen with the text : “CCS Protocol: CCS: Network timeout”. What could cause such problem?&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jul 2011 17:54:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Problems-with-development-board-MSC8156ADS/m-p/146330#M1</guid>
      <dc:creator>anis</dc:creator>
      <dc:date>2011-07-04T17:54:26Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with development board MSC8156ADS</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Problems-with-development-board-MSC8156ADS/m-p/146331#M2</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We need to make sure that the USBTAP is set up correctly for debugging.&amp;nbsp; Follow steps below:&lt;/P&gt;&lt;P&gt;1.&amp;nbsp; Start--&amp;gt;Programs--&amp;gt;Freescale CodeWarrior --&amp;gt;CodeWarrior for StarCore --&amp;gt;CodeWarrior Connection Server.&amp;nbsp; The CodeWarrior Connection Server window appears in the system toolbar.&lt;/P&gt;&lt;P&gt;2.&amp;nbsp; Double-click on CodeWarrior Connection Server icon.&amp;nbsp; The CodeWarrior Connection Server window appears.&lt;/P&gt;&lt;P&gt;3.&amp;nbsp; Type show cc -- display the correctly configured device&lt;/P&gt;&lt;P&gt;4.&amp;nbsp; Type delete all -- delete configured devices.&lt;/P&gt;&lt;P&gt;5.&amp;nbsp; Type show cc -- display the correctly configured devices.&amp;nbsp; At this point it should say that there are no command converter configured.&lt;/P&gt;&lt;P&gt;6.&amp;nbsp; Type config cc utap&lt;/P&gt;&lt;P&gt;7.&amp;nbsp; Type show cc --&amp;gt;It should state that it is sending code to the USB TAP.&lt;/P&gt;&lt;P&gt;8.&amp;nbsp; Try to debug your application.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Jul 2011 22:07:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-StarCore/Problems-with-development-board-MSC8156ADS/m-p/146331#M2</guid>
      <dc:creator>Irene</dc:creator>
      <dc:date>2011-07-06T22:07:31Z</dc:date>
    </item>
  </channel>
</rss>