<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error in downloading program into Internal Flash of M5282EVB in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137716#M891</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Why are you using a separate Flash programming application?&lt;BR /&gt;&lt;BR /&gt;Also, when you select Debug for CodeWarrior, what address is it pointing to? Next, take a look at the instruction at that address as hexadecimal data. I'd be willing to bet there's nothing but zeros in there or nonsense rather than a valid instruction or address. It appears that whatever the external Flash programmer is doing, it's not setting up a pointer to the actual starting address of your routine. The processor gets lost and triggers an exception.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 May 2006 21:06:20 GMT</pubDate>
    <dc:creator>J2MEJediMaster</dc:creator>
    <dc:date>2006-05-31T21:06:20Z</dc:date>
    <item>
      <title>Error in downloading program into Internal Flash of M5282EVB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137715#M890</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;Hi,&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;In the M5282EVB Evaluation Board, I need to execute a simple helloworld program by downloading to Internal Flash.&lt;BR /&gt;I compiled the program using the selection as M5282EVB Internal ROM.&lt;BR /&gt;Modified the M5282EVB_INT_ROM.lcf,&lt;BR /&gt;Modified TEXT (RX) : ORIGIN = 0xF0000000, (Instead of the 0x00000000)&lt;BR /&gt;Also, __FLASH = 0xF0000000.&lt;/DIV&gt;&lt;DIV&gt;I am using an external CF FLasher software.&lt;BR /&gt;Set the Target Configuration = M5282EVB(CFM)&lt;BR /&gt;FLASHBAR = 0xF0000000, BDM Communication = PE_LPT.&lt;/DIV&gt;&lt;DIV&gt;I erased the Flash contents and loaded the new program.&lt;/DIV&gt;&lt;DIV&gt;When i select Debug on the Codewarrior, it goes to the starting instruction of&lt;BR /&gt;asm_startmeup (On the codewarrior IDE, the instruction that is shown is ori.b #0x0,d0).&lt;BR /&gt;And then subsequently it jumps to the asm_exception_handler. Am i missing something?&lt;/DIV&gt;&lt;DIV&gt;Can you please help me out..&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;But, in the dBug Prompt when i say go 0xF0000F38 (which is the starting address of asm_startmeup), it displays the message &lt;A href="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif"&gt;&lt;IMG alt=":smileyhappy:" class="emoticon emoticon-smileyhappy" src="http://freescale.i.lithium.com/i/smilies/16x16_smiley-happy.gif" title="Smiley Happy" /&gt;&lt;/A&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;BR /&gt;TTA&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2006 19:23:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137715#M890</guid>
      <dc:creator>TTA</dc:creator>
      <dc:date>2006-05-31T19:23:37Z</dc:date>
    </item>
    <item>
      <title>Re: Error in downloading program into Internal Flash of M5282EVB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137716#M891</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Why are you using a separate Flash programming application?&lt;BR /&gt;&lt;BR /&gt;Also, when you select Debug for CodeWarrior, what address is it pointing to? Next, take a look at the instruction at that address as hexadecimal data. I'd be willing to bet there's nothing but zeros in there or nonsense rather than a valid instruction or address. It appears that whatever the external Flash programmer is doing, it's not setting up a pointer to the actual starting address of your routine. The processor gets lost and triggers an exception.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 May 2006 21:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137716#M891</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2006-05-31T21:06:20Z</dc:date>
    </item>
    <item>
      <title>Re: Error in downloading program into Internal Flash of M5282EVB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137717#M892</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Now, I used the Flash Programming software in the codewarrior to flash the internal flash.&lt;BR /&gt;Below are the settings in the Flash Programmer software:&lt;/P&gt;&lt;P&gt;Target Configuration:&lt;BR /&gt;=====================&lt;BR /&gt;Target Initialization: Used the file MCF5282C3_PnE.cfg&lt;/P&gt;&lt;P&gt;Target RAM Memory Buffer: 0x00000000 , Size = 0x00006000&lt;/P&gt;&lt;P&gt;Flash Configuration:&lt;BR /&gt;====================&lt;/P&gt;&lt;P&gt;Flash Memory Base Address: 0xF0000000&lt;BR /&gt;Device: M5282_CFM&lt;/P&gt;&lt;P&gt;Program/Verify:&lt;BR /&gt;===============&lt;/P&gt;&lt;P&gt;Selected file (The S19 file that i generated)&lt;BR /&gt;Restrict Address Range from F0000000 to F007FFFF.&lt;/P&gt;&lt;P&gt;I am able to erase the Flash contents and Program successfully.&lt;BR /&gt;When i Debug (in codewarrior) it goes to the starting location of asm_startmeup, but the data is junk (00000000) in that.&lt;BR /&gt;And then it jumps to asm_exceptionhandler.&lt;/P&gt;&lt;P&gt;So, i went to the dBug prompt and said go 0xF0001118 (Which was the starting location it showed when i said debug in prev step).Iam able to execute the application.&lt;/P&gt;&lt;P&gt;I have the following questions.&lt;/P&gt;&lt;P&gt;1. Any reason, why i am not able to debug in code warrior.&lt;/P&gt;&lt;P&gt;2. If i need to boot from the internal flash, what should i do? I set the SW1-8 and 9 to OFF (Internal 32-bit) and restarted the evaluation board, the execution must have started. It did not happen.&lt;/P&gt;&lt;P&gt;3. Any jumper settings need to be done?.&lt;BR /&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Jun 2006 21:31:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137717#M892</guid>
      <dc:creator>TTA</dc:creator>
      <dc:date>2006-06-01T21:31:14Z</dc:date>
    </item>
    <item>
      <title>Re: Error in downloading program into Internal Flash of M5282EVB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137718#M893</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Now, I used the Flash Programming software in the codewarrior to flash the internal flash.&lt;BR /&gt;Below are the settings in the Flash Programmer software:&lt;/P&gt;&lt;P&gt;Target Configuration:&lt;BR /&gt;=====================&lt;BR /&gt;Target Initialization: Used the file MCF5282C3_PnE.cfg&lt;/P&gt;&lt;P&gt;Target RAM Memory Buffer: 0x00000000 , Size = 0x00006000&lt;/P&gt;&lt;P&gt;Flash Configuration:&lt;BR /&gt;====================&lt;/P&gt;&lt;P&gt;Flash Memory Base Address: 0xF0000000&lt;BR /&gt;Device: M5282_CFM&lt;/P&gt;&lt;P&gt;Program/Verify:&lt;BR /&gt;===============&lt;/P&gt;&lt;P&gt;Selected file (The S19 file that i generated)&lt;BR /&gt;Restrict Address Range from F0000000 to F007FFFF.&lt;/P&gt;&lt;P&gt;I am able to erase the Flash contents and Program successfully.&lt;BR /&gt;When i Debug (in codewarrior) it goes to the starting location of asm_startmeup, but the data is junk (00000000) in that.&lt;BR /&gt;And then it jumps to asm_exceptionhandler.&lt;/P&gt;&lt;P&gt;So, i went to the dBug prompt and said go 0xF0001118 (Which was the starting location it showed when i said debug in prev step).Iam able to execute the application.&lt;/P&gt;&lt;P&gt;I have the following questions.&lt;/P&gt;&lt;P&gt;1. Any reason, why i am not able to debug in code warrior.&lt;/P&gt;&lt;P&gt;2. If i need to boot from the internal flash, what should i do? I set the SW1-8 and 9 to OFF (Internal 32-bit) and restarted the evaluation board, the execution must have started. It did not happen.&lt;/P&gt;&lt;P&gt;3. Any jumper settings need to be done?.&lt;BR /&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2006 09:51:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137718#M893</guid>
      <dc:creator>TTA</dc:creator>
      <dc:date>2006-06-02T09:51:29Z</dc:date>
    </item>
    <item>
      <title>Re: Error in downloading program into Internal Flash of M5282EVB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137719#M894</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;I'm not familiar with this particular processor, but it seems to me that the starting point of your firmware ought to have the address of your startup routine. If the Debugger is going to 0xF0000000, it's expecting a jump instruction or an address vector there that points to your routine at 0xF0000F38. As you've indicated, there's nothing there. Look at some other example programs and see how they setup the jump to the startup routine. Look at the declarations in the example code and the linker comand files carefully.&lt;BR /&gt;&lt;BR /&gt;---Tom&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jun 2006 21:27:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137719#M894</guid>
      <dc:creator>J2MEJediMaster</dc:creator>
      <dc:date>2006-06-02T21:27:45Z</dc:date>
    </item>
    <item>
      <title>Re: Error in downloading program into Internal Flash of M5282EVB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137720#M895</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I could get the program executing from Internal Flash. I had to use the CFFLasher.exe s/w for this purpose. Also the INT_ROM.lcf file need not have any changes, the TEXT location should be same i.e., 0x00000000.&lt;/P&gt;&lt;P&gt;I am not able to use the codewarrior Flash Programmer since it gives me some error. Got to check it out why? If any body has some suggestions please let me know.&lt;/P&gt;&lt;P&gt;Also, I am able to debug from Codewarrior. Thanks for all help.&lt;/P&gt;&lt;P&gt;TTA&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Jun 2006 14:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Error-in-downloading-program-into-Internal-Flash-of-M5282EVB/m-p/137720#M895</guid>
      <dc:creator>TTA</dc:creator>
      <dc:date>2006-06-07T14:16:29Z</dc:date>
    </item>
  </channel>
</rss>