<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: DDR3 MEMORY CONTENT ARE ZERO WHEN CONNECT VIA CODE WARRIER  in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708052#M6471</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian!&lt;/P&gt;&lt;P&gt;I checked that the init file run during connect but content in ddr memory still zeroes and during download it goes to machine check error(ISR).&lt;/P&gt;&lt;P&gt;Can you say how configure any one or two of three ddr controllers using tcl script and is there any settings(config file) to set frequency of ddr(800 Mhz or less than one).&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dhanasekaran k&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Oct 2017 17:35:54 GMT</pubDate>
    <dc:creator>dhanasekaran</dc:creator>
    <dc:date>2017-10-12T17:35:54Z</dc:date>
    <item>
      <title>DDR3 MEMORY CONTENT ARE ZERO WHEN CONNECT VIA CODE WARRIER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708050#M6469</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I connect ddr3 ram using code warrier and viewing memory it shows zero instead of deadbeaf but I can run qcvs test in a fine way on ddr3 location. What will be the issue?&lt;/P&gt;&lt;P&gt;We use t4240 power pc.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Sep 2017 18:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708050#M6469</guid>
      <dc:creator>dhanasekaran</dc:creator>
      <dc:date>2017-09-19T18:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 MEMORY CONTENT ARE ZERO WHEN CONNECT VIA CODE WARRIER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708051#M6470</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check your initialization file used in CodeWarrior. Also, make sure you select the option to run the init file during connecting to the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Oct 2017 14:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708051#M6470</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2017-10-02T14:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 MEMORY CONTENT ARE ZERO WHEN CONNECT VIA CODE WARRIER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708052#M6471</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Adrian!&lt;/P&gt;&lt;P&gt;I checked that the init file run during connect but content in ddr memory still zeroes and during download it goes to machine check error(ISR).&lt;/P&gt;&lt;P&gt;Can you say how configure any one or two of three ddr controllers using tcl script and is there any settings(config file) to set frequency of ddr(800 Mhz or less than one).&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Dhanasekaran k&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Oct 2017 17:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708052#M6471</guid>
      <dc:creator>dhanasekaran</dc:creator>
      <dc:date>2017-10-12T17:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 MEMORY CONTENT ARE ZERO WHEN CONNECT VIA CODE WARRIER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708053#M6472</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Check in initialization file with what value is ddr configured. In initialization file is an example of configure 2 ddr controllers. You can use this example for your case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adrian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Oct 2017 12:22:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708053#M6472</guid>
      <dc:creator>addiyi</dc:creator>
      <dc:date>2017-10-13T12:22:56Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 MEMORY CONTENT ARE ZERO WHEN CONNECT VIA CODE WARRIER</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708054#M6473</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;I tried configure only 2 DDR Controller with following configuraion values using Tcl script.I can see DDR values of mine using Register View in codewarrior after initialization. But the contrent of memory always zero (unchanged);&lt;/P&gt;&lt;P&gt;when I comment one Timing Register it shows like ?????? in memory Browser.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;# DDR1 Controller Setup&lt;BR /&gt; # DDR1_DDR_SDRAM_CFG&lt;BR /&gt; mem [CCSR_ADDR 0x8110] = 0x67040000&lt;BR /&gt; # DDR1_CS0_BNDS&lt;BR /&gt; mem [CCSR_ADDR 0x8000] = 0x0000007f&lt;BR /&gt; # DDR1_CS1_BNDS&lt;BR /&gt; mem [CCSR_ADDR 0x8008] = 0x00000000&lt;BR /&gt; # DDR1_CS2_CONFIG&lt;BR /&gt; # mem [CCSR_ADDR 0x8088] = 0xffffffff&lt;BR /&gt; # DDR1_CS3_BNDS&lt;BR /&gt; # mem [CCSR_ADDR 0x808C] = 0xffffffff&lt;BR /&gt; # DDR1_CS0_CONFIG&lt;BR /&gt; mem [CCSR_ADDR 0x8080] = 0x80044402&lt;BR /&gt; # DDR1_CS1_CONFIG&lt;BR /&gt; mem [CCSR_ADDR 0x8084] = 0x00000000&lt;BR /&gt; # DDR1_CS0_CONFIG_2&lt;BR /&gt; mem [CCSR_ADDR 0x80C0] = 0x00000000&lt;BR /&gt; # DDR1_TIMING_CFG_0&lt;BR /&gt; mem [CCSR_ADDR 0x8104] = 0x5011010C&lt;BR /&gt; # DDR1_TIMING_CFG_1&lt;BR /&gt; mem [CCSR_ADDR 0x8108] = 0xBCB40C66&lt;BR /&gt; # DDR1_TIMING_CFG_2&lt;BR /&gt; mem [CCSR_ADDR 0x810C] = 0x0040C160&lt;BR /&gt; # DDR1_TIMING_CFG_3&lt;BR /&gt; mem [CCSR_ADDR 0x8100] = 0x01111000&lt;BR /&gt; # DDR1_DDR_SDRAM_CFG_2&lt;BR /&gt; mem [CCSR_ADDR 0x8114] = 0x24401110&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE&lt;BR /&gt; mem [CCSR_ADDR 0x8118] = 0x00441C70&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_2&lt;BR /&gt; mem [CCSR_ADDR 0x811C] = 0x00980000&lt;BR /&gt; # DDR1_DDR_SDRAM_INTERVAL&lt;BR /&gt; mem [CCSR_ADDR 0x8124] = 0x0C30030C&lt;BR /&gt; # DDR1_DDR_DATA_INIT&lt;BR /&gt; mem [CCSR_ADDR 0x8128] = 0xDEADBEEF&lt;BR /&gt; # DDR1_DDR_SDRAM_CLK_CNTL&lt;BR /&gt; mem [CCSR_ADDR 0x8130] = 0x02800000&lt;BR /&gt; # DDR1_DDR_INIT_ADDR&lt;BR /&gt; mem [CCSR_ADDR 0x8148] = 0x00000000&lt;BR /&gt; # DDR1_DDR_INIT_EXT_ADDRESS&lt;BR /&gt; mem [CCSR_ADDR 0x814C] = 0x00000000&lt;BR /&gt; # DDR1_TIMING_CFG_4&lt;BR /&gt; mem [CCSR_ADDR 0x8160] = 0x00000001&lt;BR /&gt; # DDR1_TIMING_CFG_5&lt;BR /&gt; mem [CCSR_ADDR 0x8164] = 0x04401400&lt;BR /&gt; # DDR1_DDR_ZQ_CNTL&lt;BR /&gt; mem [CCSR_ADDR 0x8170] = 0x89080600&lt;BR /&gt; # DDR1_DDR_WRLVL_CNTL&lt;BR /&gt; mem [CCSR_ADDR 0x8174] = 0x8675F608&lt;BR /&gt; # DDR1_DDR_WRLVL_CNTL_2&lt;BR /&gt; mem [CCSR_ADDR 0x8190] = 0x080A0A0C&lt;BR /&gt; # DDR1_DDR_WRLVL_CNTL_3&lt;BR /&gt; mem [CCSR_ADDR 0x8194] = 0x0C0D0E0A&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_3&lt;BR /&gt; mem [CCSR_ADDR 0x8200] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_4&lt;BR /&gt; mem [CCSR_ADDR 0x8204] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_5&lt;BR /&gt; mem [CCSR_ADDR 0x8208] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_6&lt;BR /&gt; mem [CCSR_ADDR 0x820C] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_7&lt;BR /&gt; mem [CCSR_ADDR 0x8210] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_8&lt;BR /&gt; mem [CCSR_ADDR 0x8214] = 0x00000000&lt;BR /&gt; # DDR1_DDRDSR_1&lt;BR /&gt; mem [CCSR_ADDR 0x8B20] = 0x00008080&lt;BR /&gt; # DDR1_DDRDSR_2&lt;BR /&gt; mem [CCSR_ADDR 0x8B24] = 0x80000000&lt;BR /&gt; # DDR1_DDRCDR_1&lt;BR /&gt; mem [CCSR_ADDR 0x8B28] = 0x80040000&lt;BR /&gt; # DDR1_DDRCDR_2&lt;BR /&gt; mem [CCSR_ADDR 0x8B2C] = 0x00000001&lt;BR /&gt; # DDR1_ERR_DISABLE - DISABLE&lt;BR /&gt; mem [CCSR_ADDR 0x8E44] = 0x00000000&lt;BR /&gt; # DDR1_ERR_SBE&lt;BR /&gt; mem [CCSR_ADDR 0x8E58] = 0x00000000&lt;/P&gt;&lt;P&gt;# DDR2 Controller Setup&lt;BR /&gt; # DDR2_DDR_SDRAM_CFG&lt;BR /&gt; mem [CCSR_ADDR 0x9110] = 0x67040000&lt;BR /&gt; # DDR1_CS0_BNDS&lt;BR /&gt; mem [CCSR_ADDR 0x9000] = 0x008000FF&lt;BR /&gt; # DDR1_CS1_BNDS&lt;BR /&gt; mem [CCSR_ADDR 0x9008] = 0x00000000&lt;BR /&gt; # DDR1_CS2_CONFIG&lt;BR /&gt; # mem [CCSR_ADDR 0x9088] = 0xffffffff&lt;BR /&gt; # DDR1_CS3_BNDS&lt;BR /&gt; # mem [CCSR_ADDR 0x908C] = 0xffffffff&lt;BR /&gt; # DDR1_CS0_CONFIG&lt;BR /&gt; mem [CCSR_ADDR 0x9080] = 0x80044402&lt;BR /&gt; # DDR1_CS1_CONFIG&lt;BR /&gt; mem [CCSR_ADDR 0x9084] = 0x00000000&lt;BR /&gt; # DDR1_CS0_CONFIG_2&lt;BR /&gt; mem [CCSR_ADDR 0x90C0] = 0x00000000&lt;BR /&gt; # DDR1_TIMING_CFG_0&lt;BR /&gt; mem [CCSR_ADDR 0x9104] = 0x5011010C&lt;BR /&gt; # DDR1_TIMING_CFG_1&lt;BR /&gt; mem [CCSR_ADDR 0x9108] = 0xBCB40C66&lt;BR /&gt; # DDR1_TIMING_CFG_2&lt;BR /&gt; mem [CCSR_ADDR 0x910C] = 0x0040C160&lt;BR /&gt; # DDR1_TIMING_CFG_3&lt;BR /&gt; mem [CCSR_ADDR 0x9100] = 0x01111000&lt;BR /&gt; # DDR1_DDR_SDRAM_CFG_2&lt;BR /&gt; mem [CCSR_ADDR 0x9114] = 0x24401110&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE&lt;BR /&gt; mem [CCSR_ADDR 0x9118] = 0x00441C70&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_2&lt;BR /&gt; mem [CCSR_ADDR 0x911C] = 0x00980000&lt;BR /&gt; # DDR1_DDR_SDRAM_INTERVAL&lt;BR /&gt; mem [CCSR_ADDR 0x9124] = 0x0C30030C&lt;BR /&gt; # DDR1_DDR_DATA_INIT&lt;BR /&gt; mem [CCSR_ADDR 0x9128] = 0xDEADBEEF&lt;BR /&gt; # DDR1_DDR_SDRAM_CLK_CNTL&lt;BR /&gt; mem [CCSR_ADDR 0x9130] = 0x02800000&lt;BR /&gt; # DDR1_DDR_INIT_ADDR&lt;BR /&gt; mem [CCSR_ADDR 0x9148] = 0x00000000&lt;BR /&gt; # DDR1_DDR_INIT_EXT_ADDRESS&lt;BR /&gt; mem [CCSR_ADDR 0x914C] = 0x00000000&lt;BR /&gt; # DDR1_TIMING_CFG_4&lt;BR /&gt; mem [CCSR_ADDR 0x9160] = 0x00000001&lt;BR /&gt; # DDR1_TIMING_CFG_5&lt;BR /&gt; mem [CCSR_ADDR 0x9164] = 0x04401400&lt;BR /&gt; # DDR1_DDR_ZQ_CNTL&lt;BR /&gt; mem [CCSR_ADDR 0x9170] = 0x89080600&lt;BR /&gt; # DDR1_DDR_WRLVL_CNTL&lt;BR /&gt; mem [CCSR_ADDR 0x9174] = 0x8675F608&lt;BR /&gt; # DDR1_DDR_WRLVL_CNTL_2&lt;BR /&gt; mem [CCSR_ADDR 0x9190] = 0x080A0A0C&lt;BR /&gt; # DDR1_DDR_WRLVL_CNTL_3&lt;BR /&gt; mem [CCSR_ADDR 0x9194] = 0x0C0D0E0A&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_3&lt;BR /&gt; mem [CCSR_ADDR 0x9200] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_4&lt;BR /&gt; mem [CCSR_ADDR 0x9204] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_5&lt;BR /&gt; mem [CCSR_ADDR 0x9208] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_6&lt;BR /&gt; mem [CCSR_ADDR 0x920C] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_7&lt;BR /&gt; mem [CCSR_ADDR 0x9210] = 0x00000000&lt;BR /&gt; # DDR1_DDR_SDRAM_MODE_8&lt;BR /&gt; mem [CCSR_ADDR 0x9214] = 0x00000000&lt;BR /&gt; # DDR1_DDRDSR_1&lt;BR /&gt; mem [CCSR_ADDR 0x9B20] = 0x00008080&lt;BR /&gt; # DDR1_DDRDSR_2&lt;BR /&gt; mem [CCSR_ADDR 0x9B24] = 0x80000000&lt;BR /&gt; # DDR1_DDRCDR_1&lt;BR /&gt; mem [CCSR_ADDR 0x9B28] = 0x80040000&lt;BR /&gt; # DDR1_DDRCDR_2&lt;BR /&gt; mem [CCSR_ADDR 0x9B2C] = 0x00000001&lt;BR /&gt; # DDR1_ERR_DISABLE - DISABLE&lt;BR /&gt; mem [CCSR_ADDR 0x9E44] = 0x00000000&lt;BR /&gt; # DDR1_ERR_SBE&lt;BR /&gt; mem [CCSR_ADDR 0x9E58] = 0x00000000&lt;BR /&gt; &lt;BR /&gt; # DDR3 Controller Setup&lt;BR /&gt; # DDR3_DDR_SDRAM_CFG&lt;BR /&gt; #mem [CCSR_ADDR 0xA110] = 0x67040000&lt;BR /&gt; # DDR3_CS0_BNDS&lt;BR /&gt; #mem [CCSR_ADDR 0xA000] = 0x0000017f&lt;BR /&gt; # DDR3_CS1_BNDS&lt;BR /&gt; #mem [CCSR_ADDR 0xA008] = 0x0000017f&lt;BR /&gt; # DDR3_CS2_CONFIG&lt;BR /&gt; # mem [CCSR_ADDR 0xA088] = 0xffffffff&lt;BR /&gt; # DDR3_CS3_BNDS&lt;BR /&gt; # mem [CCSR_ADDR 0xA08C] = 0xffffffff&lt;BR /&gt; # DDR3_CS0_CONFIG&lt;BR /&gt; #mem [CCSR_ADDR 0xA080] = 0x80044302&lt;BR /&gt; # DDR3_CS1_CONFIG&lt;BR /&gt; #mem [CCSR_ADDR 0xA084] = 0x80004302&lt;BR /&gt; # DDR3_CS0_CONFIG_2&lt;BR /&gt; mem [CCSR_ADDR 0xA0C0] = 0x00000000&lt;BR /&gt; # DDR3_TIMING_CFG_0&lt;BR /&gt; #mem [CCSR_ADDR 0xA104] = 0x90110004&lt;BR /&gt; # DDR3_TIMING_CFG_1&lt;BR /&gt; #mem [CCSR_ADDR 0xA108] = 0xdfd9ee57&lt;BR /&gt; # DDR3_TIMING_CFG_2&lt;BR /&gt; #mem [CCSR_ADDR 0xA10C] = 0x0048e8d8&lt;BR /&gt; # DDR3_TIMING_CFG_3&lt;BR /&gt; #mem [CCSR_ADDR 0xA100] = 0x01081000&lt;BR /&gt; # DDR3_DDR_SDRAM_CFG_2&lt;BR /&gt; #mem [CCSR_ADDR 0xA114] = 0x00401010&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE&lt;BR /&gt; #mem [CCSR_ADDR 0xA118] = 0x40441014&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE_2&lt;BR /&gt; #mem [CCSR_ADDR 0xA11C] = 0x00a00000&lt;BR /&gt; # DDR3_DDR_SDRAM_INTERVAL&lt;BR /&gt; #mem [CCSR_ADDR 0xA124] = 0x0e38038e &lt;BR /&gt; # DDR3_DDR_DATA_INIT&lt;BR /&gt; #mem [CCSR_ADDR 0xA128] = 0xDEADBEEF&lt;BR /&gt; # DDR3_DDR_SDRAM_CLK_CNTL&lt;BR /&gt; #mem [CCSR_ADDR 0xA130] = 0x02000000&lt;BR /&gt; # DDR3_DDR_INIT_ADDR&lt;BR /&gt; #mem [CCSR_ADDR 0xA148] = 0x00000000&lt;BR /&gt; # DDR3_DDR_INIT_EXT_ADDRESS&lt;BR /&gt; #mem [CCSR_ADDR 0xA14C] = 0x00000000&lt;BR /&gt; # DDR3_TIMING_CFG_4&lt;BR /&gt; #mem [CCSR_ADDR 0xA160] = 0x00000001&lt;BR /&gt; # DDR3_TIMING_CFG_5&lt;BR /&gt; #mem [CCSR_ADDR 0xA164] = 0x05401400&lt;BR /&gt; # DDR3_DDR_ZQ_CNTL&lt;BR /&gt; #mem [CCSR_ADDR 0xA170] = 0x89080600&lt;BR /&gt; # DDR3_DDR_WRLVL_CNTL&lt;BR /&gt; #mem [CCSR_ADDR 0xA174] = 0x8675f609&lt;BR /&gt; # DDR3_DDR_WRLVL_CNTL_2&lt;BR /&gt; #mem [CCSR_ADDR 0xA190] = 0x090a0b0e&lt;BR /&gt; # DDR3_DDR_WRLVL_CNTL_3&lt;BR /&gt; #mem [CCSR_ADDR 0xA194] = 0x0f11120c&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE_3&lt;BR /&gt; #mem [CCSR_ADDR 0xA200] = 0x00001014&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE_4&lt;BR /&gt; #mem [CCSR_ADDR 0xA204] = 0x00a00000&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE_5&lt;BR /&gt; #mem [CCSR_ADDR 0xA208] = 0x00001014&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE_6&lt;BR /&gt; #mem [CCSR_ADDR 0xA20C] = 0x00a00000&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE_7&lt;BR /&gt; #mem [CCSR_ADDR 0xA210] = 0x00001014&lt;BR /&gt; # DDR3_DDR_SDRAM_MODE_8&lt;BR /&gt; #mem [CCSR_ADDR 0xA214] = 0x00a00000&lt;BR /&gt; # DDR3_DDRDSR_1&lt;BR /&gt; #mem [CCSR_ADDR 0xAB20] = 0x00008080&lt;BR /&gt; # DDR3_DDRDSR_2&lt;BR /&gt; #mem [CCSR_ADDR 0xAB24] = 0x80000000&lt;BR /&gt; # DDR3_DDRCDR_1&lt;BR /&gt; #mem [CCSR_ADDR 0xAB28] = 0x80040000&lt;BR /&gt; # DDR3_DDRCDR_2&lt;BR /&gt; #mem [CCSR_ADDR 0xAB2C] = 0x00000001&lt;BR /&gt; # DDR3_ERR_DISABLE - DISABLE&lt;BR /&gt; #mem [CCSR_ADDR 0xAE44] = 0x00000000&lt;BR /&gt; # DDR3_ERR_SBE&lt;BR /&gt; #mem [CCSR_ADDR 0xAE58] = 0x00000000&lt;/P&gt;&lt;P&gt;wait 100&lt;BR /&gt; # DDR1_DDR_SDRAM_CFG&lt;BR /&gt; mem [CCSR_ADDR 0x8110] = 0xC70C0000&lt;BR /&gt; # DDR2_DDR_SDRAM_CFG&lt;BR /&gt; mem [CCSR_ADDR 0x9110] = 0xC70C0000&lt;BR /&gt; # DDR3_DDR_SDRAM_CFG&lt;BR /&gt; #mem [CCSR_ADDR 0xa110] = 0x67040000&lt;BR /&gt; wait 1000 &lt;BR /&gt; # DDR1_ERR_DISABLE - ENABLE&lt;BR /&gt; mem [CCSR_ADDR 0x8E44] = 0x00000000&lt;BR /&gt; # DDR2_ERR_DISABLE - ENABLE&lt;BR /&gt; mem [CCSR_ADDR 0x9E44] = 0x00000000&lt;BR /&gt; # DDR3_ERR_DISABLE - ENABLE&lt;BR /&gt; #mem [CCSR_ADDR 0xaE44] = 0x00000000&lt;/P&gt;&lt;P&gt;# CCF_MCINTLV3R - enable 3-way interleaving&lt;BR /&gt; # CCF_MCINTLV3R[27–31]: GRANULE_SIZE&lt;BR /&gt; # 01010 1 KB granule size&lt;BR /&gt; # 01100 4 KB granule size&lt;BR /&gt; # 01101 8 KB granule size&lt;BR /&gt; #mem [CCSR_ADDR 0x18004] = 0x800000[format %02x [format %.0f [expr 10 + [logToBaseTwo $GRANULE_SIZE]]]]&lt;BR /&gt; mem [CCSR_ADDR 0x18004] = 0xc&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;dhanasekaran K.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 14 Oct 2017 09:40:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/DDR3-MEMORY-CONTENT-ARE-ZERO-WHEN-CONNECT-VIA-CODE-WARRIER/m-p/708054#M6473</guid>
      <dc:creator>dhanasekaran</dc:creator>
      <dc:date>2017-10-14T09:40:42Z</dc:date>
    </item>
  </channel>
</rss>