<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Boot from P1024RDB NOR Flash in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Boot-from-P1024RDB-NOR-Flash/m-p/683748#M6387</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to boot u-boot.bin on the P1024RDB from the NOR Flash using the CodeWarrior TAP. I tried the same for the NOR Flash middle sectors and was successful in burning the image onto the NOR Flash's middle sectors and could successfully boot the same. But when I changed SW4[8] to off and tried flashing the same I could burn the image, but it doesn't boot. (for the middle sectors boot the address offset I configured was 0xfff80000) Also the base address by default while using the configuration .xml file for the P1024_NOR_Flash.xml is 0xFF000000.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What should be the address offset for the booting from the upper 4 sectors ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;P.S - I'm using the CodeWarrior IDE v10.5.1 for Power Architecture on a Linux machine&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Jul 2017 11:11:35 GMT</pubDate>
    <dc:creator>pavankumarg</dc:creator>
    <dc:date>2017-07-26T11:11:35Z</dc:date>
    <item>
      <title>Boot from P1024RDB NOR Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Boot-from-P1024RDB-NOR-Flash/m-p/683748#M6387</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want to boot u-boot.bin on the P1024RDB from the NOR Flash using the CodeWarrior TAP. I tried the same for the NOR Flash middle sectors and was successful in burning the image onto the NOR Flash's middle sectors and could successfully boot the same. But when I changed SW4[8] to off and tried flashing the same I could burn the image, but it doesn't boot. (for the middle sectors boot the address offset I configured was 0xfff80000) Also the base address by default while using the configuration .xml file for the P1024_NOR_Flash.xml is 0xFF000000.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;What should be the address offset for the booting from the upper 4 sectors ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;P.S - I'm using the CodeWarrior IDE v10.5.1 for Power Architecture on a Linux machine&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jul 2017 11:11:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Boot-from-P1024RDB-NOR-Flash/m-p/683748#M6387</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-07-26T11:11:35Z</dc:date>
    </item>
    <item>
      <title>Re: Boot from P1024RDB NOR Flash</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Boot-from-P1024RDB-NOR-Flash/m-p/683749#M6388</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="296942" data-username="pavankumarg" href="https://community.nxp.com/people/pavankumarg"&gt;Pavankumar G&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The address 0xfff80000 should also been used &lt;SPAN&gt;for the upper 4 sectors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Please create a project with Attach launch configuration enabled, then connect to the target board with Attach launch configuration to check what disassembly code would be captured in CodeWarrior IDE.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Aug 2017 08:51:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Boot-from-P1024RDB-NOR-Flash/m-p/683749#M6388</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-08-16T08:51:59Z</dc:date>
    </item>
  </channel>
</rss>