<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Writing driver codes on Yocto's layer or creating a higher level layer that includes meta-ppc in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Writing-driver-codes-on-Yocto-s-layer-or-creating-a-higher-level/m-p/637932#M6226</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my Yocto project,I want to implement my driver codes to Yocto's layer.I use T1024rdbfor this purpose which has power pc architecture.So,in Yocto I think that meta-ppc layer is suitable for this purpose;on the other hand,creating a higher level layer which&amp;nbsp;includes meta-ppc can give me the advantage of using&amp;nbsp;also meta-ppc layer's&amp;nbsp;properties.So,is it&amp;nbsp;possible to create a new higher level layer which includes this meta-ppc layer or any documents,references or manuals about this topic?or could you recommend something about this issue?&lt;/P&gt;&lt;P&gt;Thanks for your answers.&lt;/P&gt;&lt;P&gt;Best Regards...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Feb 2017 07:29:42 GMT</pubDate>
    <dc:creator>cengizhanyapici</dc:creator>
    <dc:date>2017-02-15T07:29:42Z</dc:date>
    <item>
      <title>Writing driver codes on Yocto's layer or creating a higher level layer that includes meta-ppc</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Writing-driver-codes-on-Yocto-s-layer-or-creating-a-higher-level/m-p/637932#M6226</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my Yocto project,I want to implement my driver codes to Yocto's layer.I use T1024rdbfor this purpose which has power pc architecture.So,in Yocto I think that meta-ppc layer is suitable for this purpose;on the other hand,creating a higher level layer which&amp;nbsp;includes meta-ppc can give me the advantage of using&amp;nbsp;also meta-ppc layer's&amp;nbsp;properties.So,is it&amp;nbsp;possible to create a new higher level layer which includes this meta-ppc layer or any documents,references or manuals about this topic?or could you recommend something about this issue?&lt;/P&gt;&lt;P&gt;Thanks for your answers.&lt;/P&gt;&lt;P&gt;Best Regards...&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Feb 2017 07:29:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Writing-driver-codes-on-Yocto-s-layer-or-creating-a-higher-level/m-p/637932#M6226</guid>
      <dc:creator>cengizhanyapici</dc:creator>
      <dc:date>2017-02-15T07:29:42Z</dc:date>
    </item>
    <item>
      <title>Re: Writing driver codes on Yocto's layer or creating a higher level layer that includes meta-ppc</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Writing-driver-codes-on-Yocto-s-layer-or-creating-a-higher-level/m-p/637933#M6227</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="293839" data-username="cengizhanyapicioglu" href="https://community.nxp.com/people/cengizhanyapicioglu"&gt;Cengizhan Yapicioglu&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For create a custom layer, you could refer to &lt;A class="link-titled" href="https://github.com/yoctocookbook/meta-custom" title="https://github.com/yoctocookbook/meta-custom"&gt;GitHub - yoctocookbook/meta-custom: Example meta-custom Yocto layer&lt;/A&gt;&amp;nbsp;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The attached is an example about how meta-freescale including dynamic-layers layer, please pay attention to meta-freescale_bak/conf/layer.conf configuration, especially BBFILES variable definition.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Feb 2017 09:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Writing-driver-codes-on-Yocto-s-layer-or-creating-a-higher-level/m-p/637933#M6227</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-02-22T09:15:26Z</dc:date>
    </item>
  </channel>
</rss>