<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Connecting to Coldfire target without downloading program in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Connecting-to-Coldfire-target-without-downloading-program/m-p/203848#M4219</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes, this is possible. It is named 'CodeWarrior Attach' in CodeWarrior for MCU10.x. See attached screenshot.&lt;/P&gt;&lt;P&gt;Althoug on ColdFire V2 it will stop the target on attach. But it will not download or initialize it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"CodeWarrior Attach": you have a project and the sources for the application you want to do a hotsync. That allows you source level debugging&lt;/P&gt;&lt;P&gt;"CodeWarrior Connect": here you do not have the sources/project/binaries on the host: means you do a hotsync and then you can debug it with what you have.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 08 Feb 2012 16:07:48 GMT</pubDate>
    <dc:creator>BlackNight</dc:creator>
    <dc:date>2012-02-08T16:07:48Z</dc:date>
    <item>
      <title>Connecting to Coldfire target without downloading program</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Connecting-to-Coldfire-target-without-downloading-program/m-p/203847#M4218</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The 8-bit S08 parts have the capability of connecting to a running micro without stopping or resetting it (Hotsync).&amp;nbsp; Is this possible with a ColdFire V2 target?&amp;nbsp; If there is a way to "Hotsync" with a V2 ColdFire, where is it documented?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2012 05:30:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Connecting-to-Coldfire-target-without-downloading-program/m-p/203847#M4218</guid>
      <dc:creator>kecart</dc:creator>
      <dc:date>2012-02-08T05:30:26Z</dc:date>
    </item>
    <item>
      <title>Re: Connecting to Coldfire target without downloading program</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Connecting-to-Coldfire-target-without-downloading-program/m-p/203848#M4219</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;yes, this is possible. It is named 'CodeWarrior Attach' in CodeWarrior for MCU10.x. See attached screenshot.&lt;/P&gt;&lt;P&gt;Althoug on ColdFire V2 it will stop the target on attach. But it will not download or initialize it.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"CodeWarrior Attach": you have a project and the sources for the application you want to do a hotsync. That allows you source level debugging&lt;/P&gt;&lt;P&gt;"CodeWarrior Connect": here you do not have the sources/project/binaries on the host: means you do a hotsync and then you can debug it with what you have.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope this helps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Feb 2012 16:07:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Connecting-to-Coldfire-target-without-downloading-program/m-p/203848#M4219</guid>
      <dc:creator>BlackNight</dc:creator>
      <dc:date>2012-02-08T16:07:48Z</dc:date>
    </item>
  </channel>
</rss>