<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic &amp;quot;Core not responding&amp;quot; when programing MPC8377 in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/quot-Core-not-responding-quot-when-programing-MPC8377/m-p/201684#M4100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using codewarrior windows version to program MPC8377. The codewarrior version is the newest 8.8.2. I use M29W640GT flash instead of S29GL064R3 on board. But error happens when programing flash like:&lt;/P&gt;&lt;P&gt;Programming 0x00010000 bytes of Target Memory at 0xFE000000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE010000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE020000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE030000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE040000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE050000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE060000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE070000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE080000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE090000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE0A0000&lt;BR /&gt;Flash Programmer: CCSProtocolPlugin : Failed to continue thread [Core not responding]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The stop address will change every time. And I can use u-boot to program flash correctlly. So it seems that&amp;nbsp;something is wrong with codewarrior or USBTAP. Could someone helps me to solve the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 Jul 2009 12:17:03 GMT</pubDate>
    <dc:creator>alerk03</dc:creator>
    <dc:date>2009-07-22T12:17:03Z</dc:date>
    <item>
      <title>"Core not responding" when programing MPC8377</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/quot-Core-not-responding-quot-when-programing-MPC8377/m-p/201684#M4100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using codewarrior windows version to program MPC8377. The codewarrior version is the newest 8.8.2. I use M29W640GT flash instead of S29GL064R3 on board. But error happens when programing flash like:&lt;/P&gt;&lt;P&gt;Programming 0x00010000 bytes of Target Memory at 0xFE000000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE010000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE020000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE030000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE040000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE050000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE060000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE070000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE080000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE090000&lt;BR /&gt;Programming 0x00010000 bytes of Target Memory at 0xFE0A0000&lt;BR /&gt;Flash Programmer: CCSProtocolPlugin : Failed to continue thread [Core not responding]&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The stop address will change every time. And I can use u-boot to program flash correctlly. So it seems that&amp;nbsp;something is wrong with codewarrior or USBTAP. Could someone helps me to solve the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2009 12:17:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/quot-Core-not-responding-quot-when-programing-MPC8377/m-p/201684#M4100</guid>
      <dc:creator>alerk03</dc:creator>
      <dc:date>2009-07-22T12:17:03Z</dc:date>
    </item>
    <item>
      <title>Re: "Core not responding" when programing MPC8377</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/quot-Core-not-responding-quot-when-programing-MPC8377/m-p/201685#M4101</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In situations like this, where flash-programming fails for no discernable reason, I find that slowing the Interface Clock Frequency of the USB TAP or Ethernet TAP usually helps.&amp;nbsp; From the CodeWarrior IDE Toolbar select Edit-&amp;gt;Preferences-&amp;gt;Remote Connections.&amp;nbsp; Double-click on the connection option you're using in the Flash Programmer. In the configuration panel that pops up, change the Interface Clock Frequency option to 1MHz.&amp;nbsp; You may find that faster speeds also work but start with 1MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-Ron&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2009 00:25:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/quot-Core-not-responding-quot-when-programing-MPC8377/m-p/201685#M4101</guid>
      <dc:creator>ronco</dc:creator>
      <dc:date>2009-07-30T00:25:48Z</dc:date>
    </item>
  </channel>
</rss>