<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: CodeWarrior USB TAP TX/RX Always Flashing Red in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189096#M3598</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not aware of such a document. I assume that connection server starts automatically when you try to debug with CodeWarrior? If so, it looks like that particular command is doing some sort of magic that the debugger initialization script for the P1025 lacks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 13 Sep 2012 12:16:30 GMT</pubDate>
    <dc:creator>tom_thompson</dc:creator>
    <dc:date>2012-09-13T12:16:30Z</dc:date>
    <item>
      <title>CodeWarrior USB TAP TX/RX Always Flashing Red</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189093#M3595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello -&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am new to CodeWarrior but have followed the instructions for using CodeWarrior to flash a new image to a P1025TWR system but my USB TAP is always flashing/blinking red for the TX/RX LED.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am running CodeWarrior Dev Stuidio 10.1.1&lt;/P&gt;&lt;P&gt;- Windows 7 32-bit&lt;/P&gt;&lt;P&gt;- I have run the C:\Program Files\Freescale\CW PA v10.1.1\PA\ccs\drivers\usb\setup.bat to install the latest USB driver&lt;/P&gt;&lt;P&gt;- And I have tried many steps to properly communicate over the USB interface to the USB TAP.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any thoughts or help is appreciated.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Sep 2012 23:04:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189093#M3595</guid>
      <dc:creator>joekozio</dc:creator>
      <dc:date>2012-09-10T23:04:49Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior USB TAP TX/RX Always Flashing Red</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189094#M3596</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In CodeWarrior, go to the Debug Configuration window (Run &amp;gt; Debug Configurations).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Click on your project on the left, then on the Main tab at the right. Click on Edit adjacent to the Connection option. Check to see if USB has been chosen. Under the Advanced Tab, you can Enable logging, which should give you a communications trace when you try to connect. That might shed more light on what is going on.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2012 12:00:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189094#M3596</guid>
      <dc:creator>tom_thompson</dc:creator>
      <dc:date>2012-09-12T12:00:35Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior USB TAP TX/RX Always Flashing Red</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189095#M3597</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Tom.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't say that I understand why, but I got the USB Tap connection working&lt;/P&gt;&lt;P&gt;by doing the following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attach the USB Tap to the P1025TWR JTAG header&lt;/P&gt;&lt;P&gt;Attach the USB Tap to my PC's USB port&lt;/P&gt;&lt;P&gt;Launch the CodeWarrior IDE (Version 10.1.1)&lt;/P&gt;&lt;P&gt;Launch the CodeWarrior Connection Server (Start -&amp;gt; All Programs -&amp;gt;&lt;/P&gt;&lt;P&gt;Freescale CodeWarriror -&amp;gt; CW for PA 10.1.1)&lt;/P&gt;&lt;P&gt;In the Windows 7 task bar, find the CodeWarrior Connection Server icon,&lt;/P&gt;&lt;P&gt;right-mouse, then "Show console"&lt;/P&gt;&lt;P&gt;From the CodeWarrior Connection Server console, run "show cc run" - This&lt;/P&gt;&lt;P&gt;command does something to transition the USB Code Tap TX/RX Led from&lt;/P&gt;&lt;P&gt;flashing red to flashing green. And the ready state. I can now use the CW&lt;/P&gt;&lt;P&gt;IDE, select a Target Task, Change Run Configuration to&lt;/P&gt;&lt;P&gt;1025twr_Hardware_Debug_core0_P1025_P1025RDB_Debug_Download, and Select&lt;/P&gt;&lt;P&gt;EXECUTE. This fails, but I am getting help through a SR.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Being that I like to understand why the "show cc run" gets my USB Tap&lt;/P&gt;&lt;P&gt;ready, is there docs on the commandsand perhaps you can explain?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Joe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Wed, Sep 12, 2012 at 6:00 AM, tom_thompson &amp;lt;admin@community.freescale.com&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Sep 2012 16:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189095#M3597</guid>
      <dc:creator>joekozio</dc:creator>
      <dc:date>2012-09-12T16:32:43Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior USB TAP TX/RX Always Flashing Red</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189096#M3598</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am not aware of such a document. I assume that connection server starts automatically when you try to debug with CodeWarrior? If so, it looks like that particular command is doing some sort of magic that the debugger initialization script for the P1025 lacks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;---Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Sep 2012 12:16:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/CodeWarrior-USB-TAP-TX-RX-Always-Flashing-Red/m-p/189096#M3598</guid>
      <dc:creator>tom_thompson</dc:creator>
      <dc:date>2012-09-13T12:16:30Z</dc:date>
    </item>
  </channel>
</rss>