<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Strange Problems about flash programming in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Strange-Problems-about-flash-programming/m-p/155997#M2030</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;Dear all,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;My board is based on MPC8540 processor&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;My Codewarrior is V8.8 for Powerpc and USB-TAP&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;It’s a bareboard that designed by myself, not a standard evaluation board. The flash chip is Intel’s JS28F128J3D-75. I used the Initialization File of &lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;MSC8144ADS_init.cfg successfully connected the board and erased the flash, but the weird things are that ( sometimes) I could program the flash correctly as well as validation, and the UBOOT started well after flash programming, everything was OK right then. But next day when I again booted the board I had the UBOOT unhealthy. At the very beginning, It had only several start information lines displayed in the&lt;/SPAN&gt; &lt;SPAN&gt;Terminal Emulator Window and hang up, as I restarted the board the less information displayed, and I got nothing on the terminal emulator after several times restarting the board. The UBOOT just disappeared. Then I re programmed the flash, and the error appeared when blank checking or validating. Some sectors failed to erase or program.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;It’s strange, please give me some advise.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;Since my board is not an evaluation board, must I config a new&lt;/SPAN&gt; &lt;SPAN&gt;Initialization File instead of MSC8144ADS_init.cfg that totally matching my board ? What else should I do besides Initialization File for a new designed board ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Feb 2009 13:54:00 GMT</pubDate>
    <dc:creator>jaffe</dc:creator>
    <dc:date>2009-02-25T13:54:00Z</dc:date>
    <item>
      <title>Strange Problems about flash programming</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Strange-Problems-about-flash-programming/m-p/155997#M2030</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;Dear all,&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;My board is based on MPC8540 processor&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;My Codewarrior is V8.8 for Powerpc and USB-TAP&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;It’s a bareboard that designed by myself, not a standard evaluation board. The flash chip is Intel’s JS28F128J3D-75. I used the Initialization File of &lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;MSC8144ADS_init.cfg successfully connected the board and erased the flash, but the weird things are that ( sometimes) I could program the flash correctly as well as validation, and the UBOOT started well after flash programming, everything was OK right then. But next day when I again booted the board I had the UBOOT unhealthy. At the very beginning, It had only several start information lines displayed in the&lt;/SPAN&gt; &lt;SPAN&gt;Terminal Emulator Window and hang up, as I restarted the board the less information displayed, and I got nothing on the terminal emulator after several times restarting the board. The UBOOT just disappeared. Then I re programmed the flash, and the error appeared when blank checking or validating. Some sectors failed to erase or program.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;It’s strange, please give me some advise.&lt;/SPAN&gt;&lt;/P&gt;&lt;P class="MsoNormal"&gt;&lt;SPAN&gt;Since my board is not an evaluation board, must I config a new&lt;/SPAN&gt; &lt;SPAN&gt;Initialization File instead of MSC8144ADS_init.cfg that totally matching my board ? What else should I do besides Initialization File for a new designed board ?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2009 13:54:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Strange-Problems-about-flash-programming/m-p/155997#M2030</guid>
      <dc:creator>jaffe</dc:creator>
      <dc:date>2009-02-25T13:54:00Z</dc:date>
    </item>
    <item>
      <title>Re: Strange Problems about flash programming</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Strange-Problems-about-flash-programming/m-p/155998#M2031</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It appears that the target board is occasionally not running correctly which would cause the CodeWarrior Flash Programmer to behave erratically as well.&amp;nbsp; Intermittent failures like this, especially on a new target design, could be due to overheating of the board.&amp;nbsp; Does cooling the board, either with a fan or freeze spray, improve behavior?&amp;nbsp; If so, that would be the solution.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Another approach would be to slow down the Interface Clock Frequency of your USB TAP.&amp;nbsp; In the CodeWarrior IDE select Edit-&amp;gt;Preferences-&amp;gt;Remote Connections, double-click on the USB TAP entry that you're using in the Flash Programmer, click on the pull-down menu next to the 'Interface Clock Frequency' option and select a lower value.&amp;nbsp; Start with 1Mhz and go from there.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I would also double-check the target RAM configuration in the Flash Programmer's Target Initialization (.cfg) file, perhaps selecting the slowest, most reliable RAM settings available.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2009 03:05:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/Strange-Problems-about-flash-programming/m-p/155998#M2031</guid>
      <dc:creator>ronco</dc:creator>
      <dc:date>2009-03-25T03:05:25Z</dc:date>
    </item>
  </channel>
</rss>