<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MPC8313 &amp; SPI in CodeWarrior for QorIQ</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/MPC8313-SPI/m-p/155965#M2027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to understand how the SPI interface works in this BSP.&amp;nbsp; I don't see any of the spi devices in /dev/.&amp;nbsp; Do they need to be created by hand using 'mknod'?&amp;nbsp; Are they located elsewhere?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, does anyone have some example SPI code that talks to the MPC83* SPI driver?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Feb 2009 07:14:20 GMT</pubDate>
    <dc:creator>MarkB</dc:creator>
    <dc:date>2009-02-25T07:14:20Z</dc:date>
    <item>
      <title>MPC8313 &amp; SPI</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/MPC8313-SPI/m-p/155965#M2027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to understand how the SPI interface works in this BSP.&amp;nbsp; I don't see any of the spi devices in /dev/.&amp;nbsp; Do they need to be created by hand using 'mknod'?&amp;nbsp; Are they located elsewhere?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, does anyone have some example SPI code that talks to the MPC83* SPI driver?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2009 07:14:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/MPC8313-SPI/m-p/155965#M2027</guid>
      <dc:creator>MarkB</dc:creator>
      <dc:date>2009-02-25T07:14:20Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313 &amp; SPI</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/MPC8313-SPI/m-p/155966#M2028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I've replaced my Rev A4 boards with the new Rev C hardware and I still can't get spidev up and running.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've recompiled the kernel with SPI support and I am loading devfs.&amp;nbsp; However, I see that udevd is present on the RDB but it isn't running at startup.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Do I need both devfsd and udevd?&amp;nbsp; It seems like I wouldn't.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've even tried passing mount=devfsd as a boot parameter.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;FYI, I am using the spidev_test.c compiled binary as a starter.&amp;nbsp; I always get "can't open device: No such file or directory" which suggests to me that udev or devfs is borked.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've also tried the BSP kernel and 2.6.28.6.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2009 04:42:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/MPC8313-SPI/m-p/155966#M2028</guid>
      <dc:creator>MarkB</dc:creator>
      <dc:date>2009-03-17T04:42:26Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313 &amp; SPI</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/MPC8313-SPI/m-p/155967#M2029</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hiii&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;did you find the example code for SPI. i am&amp;nbsp; struck on the same side. please tell me how to check SPI communication for MPC8313 . I am also having this BSP Pakage for Rev. 4 . how to use this. guide me all please.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Feb 2012 14:39:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/MPC8313-SPI/m-p/155967#M2029</guid>
      <dc:creator>set</dc:creator>
      <dc:date>2012-02-14T14:39:53Z</dc:date>
    </item>
  </channel>
</rss>