<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for QorIQのトピックRe: AppTRK &amp; MPC8313-RDB</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/AppTRK-MPC8313-RDB/m-p/155734#M2002</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes you can but you'll still need to install the Freescale BSP for the MPC8313-RDB to get the apptrk executable.&amp;nbsp; Download and install that BSP, run LTIB and select the apptrk package to generate the apptrk executable.&amp;nbsp; This file will be located in the {LTIB}/rootfs/usr/bin folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next step depends on how your BSP incorporates files into its root&amp;nbsp;file system.&amp;nbsp; Refer to your documentation on that if you want apptrk included in the rfs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You have a couple of other options for using apptrk with this BSP:&lt;BR /&gt;&amp;nbsp; - boot your system and then tftp or ftp apptrk to the running system.&lt;BR /&gt;&amp;nbsp; - boot your system and then NFS-mount a directory from your running system and put apptrk in that directory so it is accessable on the target board (and if you'll permit a brief editorial, NFS is still a better method than ramdisk for application development.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Apr 2009 21:07:41 GMT</pubDate>
    <dc:creator>ronco</dc:creator>
    <dc:date>2009-04-01T21:07:41Z</dc:date>
    <item>
      <title>AppTRK &amp; MPC8313-RDB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/AppTRK-MPC8313-RDB/m-p/155733#M2001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;SPAN&gt;I have a MPC8313-RDB and I am not using the BSP from Freescale.&amp;nbsp; I have it booting with kernel 2.6.28.6 and busybox.&amp;nbsp; Is there a way to get the AppTRK.elf package working in my ramdisk image?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Feb 2009 00:24:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/AppTRK-MPC8313-RDB/m-p/155733#M2001</guid>
      <dc:creator>MarkB</dc:creator>
      <dc:date>2009-02-25T00:24:19Z</dc:date>
    </item>
    <item>
      <title>Re: AppTRK &amp; MPC8313-RDB</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/AppTRK-MPC8313-RDB/m-p/155734#M2002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes you can but you'll still need to install the Freescale BSP for the MPC8313-RDB to get the apptrk executable.&amp;nbsp; Download and install that BSP, run LTIB and select the apptrk package to generate the apptrk executable.&amp;nbsp; This file will be located in the {LTIB}/rootfs/usr/bin folder.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The next step depends on how your BSP incorporates files into its root&amp;nbsp;file system.&amp;nbsp; Refer to your documentation on that if you want apptrk included in the rfs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You have a couple of other options for using apptrk with this BSP:&lt;BR /&gt;&amp;nbsp; - boot your system and then tftp or ftp apptrk to the running system.&lt;BR /&gt;&amp;nbsp; - boot your system and then NFS-mount a directory from your running system and put apptrk in that directory so it is accessable on the target board (and if you'll permit a brief editorial, NFS is still a better method than ramdisk for application development.)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Apr 2009 21:07:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-QorIQ/AppTRK-MPC8313-RDB/m-p/155734#M2002</guid>
      <dc:creator>ronco</dc:creator>
      <dc:date>2009-04-01T21:07:41Z</dc:date>
    </item>
  </channel>
</rss>