<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Import 8.3 codewarrior project into codewarrior 10.4</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254519#M9772</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please refer an4727&amp;nbsp; for how to port classic CW to eclipse:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf" title="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Aug 2013 02:09:11 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2013-08-15T02:09:11Z</dc:date>
    <item>
      <title>Import 8.3 codewarrior project into codewarrior 10.4</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254518#M9771</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Having problem importing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Aug 2013 16:45:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254518#M9771</guid>
      <dc:creator>lynnschneider</dc:creator>
      <dc:date>2013-08-14T16:45:50Z</dc:date>
    </item>
    <item>
      <title>Re: Import 8.3 codewarrior project into codewarrior 10.4</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254519#M9772</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;please refer an4727&amp;nbsp; for how to port classic CW to eclipse:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf" title="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2013 02:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254519#M9772</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2013-08-15T02:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: Import 8.3 codewarrior project into codewarrior 10.4</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254520#M9773</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What about the PE settings? Shouldn't Freescale provide a easier tool to convert?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Oct 2013 09:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254520#M9773</guid>
      <dc:creator>tonywu</dc:creator>
      <dc:date>2013-10-24T09:29:53Z</dc:date>
    </item>
    <item>
      <title>Re: Import 8.3 codewarrior project into codewarrior 10.4</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254521#M9774</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;CodeWarrior v10.5 includes CodeWarrior Classic Project Importer for CW DSC v8.3 projects, but CW v10.4 does not. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CodeWarrior v10.5 can be downloaded from: &lt;/P&gt;&lt;P&gt;&lt;A href="http://tinyurl.com/6jo5tge"&gt;http://tinyurl.com/6jo5tge&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you would use CW10.4, the solution is user needs to create a new bareboard project in CW10.4 and then add/copy all your source files to the new project.&amp;nbsp; For a project with PE, user also have to add the PE component manually.&lt;/P&gt;&lt;P&gt;Below is an application not for how to do this:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf"&gt;http://cache.freescale.com/files/soft_dev_tools/doc/app_note/AN4727.pdf&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Oct 2013 02:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254521#M9774</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2013-10-25T02:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: Import 8.3 codewarrior project into codewarrior 10.4</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254522#M9775</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I spent two hours downloading and installing version 10.5 but I can't find anything in the help system that explains how to import a project from CW 8.3.&amp;nbsp; Also in CW 8.3 it appears that the Export Project function doesn't generate anything except an xml file with some project settings.&amp;nbsp; I think I'd need more than that to import into CS 10.5.&amp;nbsp; What is the procedure for exporting from 8.3 and importing into 10.5 or where do I find this information?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Oct 2013 16:47:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254522#M9775</guid>
      <dc:creator>lancefisher</dc:creator>
      <dc:date>2013-10-25T16:47:23Z</dc:date>
    </item>
    <item>
      <title>Re: Import 8.3 codewarrior project into codewarrior 10.4</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254523#M9776</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Lance, I import old project to 10.5 directly from 10.5 menu file&amp;gt;import&lt;/P&gt;&lt;P&gt;In the selection window select the CodeWarrior folder and the "CodeWarrior Classic Project".&lt;/P&gt;&lt;P&gt;It worked for me. No special export preparations in 8.3 needed. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 26 Oct 2013 10:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Import-8-3-codewarrior-project-into-codewarrior-10-4/m-p/254523#M9776</guid>
      <dc:creator>Ben</dc:creator>
      <dc:date>2013-10-26T10:43:20Z</dc:date>
    </item>
  </channel>
</rss>