<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: Target not run after flashing</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249808#M9626</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim Donelson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my design, JTAG' reset pin is not connected to Target's reset input. &lt;/P&gt;&lt;P&gt;Normaly, must do reset action after flashing. But in this case is not such. I have to do uplug and plug again power cable so that target can run. If I connect my target to PC via RS232, it seems noisy data (or zero' value) transmitted forever. And my target is blocked&amp;nbsp; in that state.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Apr 2013 02:43:14 GMT</pubDate>
    <dc:creator>nguyenhung</dc:creator>
    <dc:date>2013-04-04T02:43:14Z</dc:date>
    <item>
      <title>Target not run after flashing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249806#M9624</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everybody,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In codewarrior, i have use 'Flash file target' function to flash target. But target does not run after flashing (even do press reset button). I have to unplug power supply and then everything is ok.&lt;/P&gt;&lt;P&gt;Anyone can explain what happened?&lt;/P&gt;&lt;P&gt;Im using CW10.2 and Multilink universal FX&amp;nbsp; debugger of PE micro.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks a lot!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2013 07:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249806#M9624</guid>
      <dc:creator>nguyenhung</dc:creator>
      <dc:date>2013-04-03T07:37:21Z</dc:date>
    </item>
    <item>
      <title>Re: Target not run after flashing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249807#M9625</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The BDM may be holding the reset line low.&lt;/P&gt;&lt;P&gt;Try unplugging the BDM after flashing.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2013 13:52:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249807#M9625</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2013-04-03T13:52:18Z</dc:date>
    </item>
    <item>
      <title>Re: Target not run after flashing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249808#M9626</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jim Donelson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my design, JTAG' reset pin is not connected to Target's reset input. &lt;/P&gt;&lt;P&gt;Normaly, must do reset action after flashing. But in this case is not such. I have to do uplug and plug again power cable so that target can run. If I connect my target to PC via RS232, it seems noisy data (or zero' value) transmitted forever. And my target is blocked&amp;nbsp; in that state.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2013 02:43:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249808#M9626</guid>
      <dc:creator>nguyenhung</dc:creator>
      <dc:date>2013-04-04T02:43:14Z</dc:date>
    </item>
    <item>
      <title>Re: Target not run after flashing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249809#M9627</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does the reset button work after cycling power?&lt;/P&gt;&lt;P&gt;Exactly how are you connecting the PC via RS232?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2013 17:34:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249809#M9627</guid>
      <dc:creator>JimDon</dc:creator>
      <dc:date>2013-04-04T17:34:47Z</dc:date>
    </item>
    <item>
      <title>Re: Target not run after flashing</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249810#M9628</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nguyen Hung.&lt;/P&gt;&lt;P&gt;Can you check in your project "Properties-&amp;gt;ARM Linker-&amp;gt;Input" the next thinks: &lt;/P&gt;&lt;P&gt;1) Linker command file is intended for your MCU: ..../MK60DN512Z_flash.lcf is intended for K60 (512K ROM/512K RAM) MCU, etc.&lt;/P&gt;&lt;P&gt;2) In "Entry Point" field you have any label name: __thumb_startup (for example). This is a ivINT_Initial_Program_Counter are placed in your vectortable in the address 0x01. Check that this label the same as in the vectortable (in kinetis_sysinit.c file).&lt;/P&gt;&lt;P&gt;3) If you work with RAM "flashing" (check that in the "Run/Debug target" is RAM or Flash) and you haven't enought RAM memory your program will not run.&lt;/P&gt;&lt;P&gt;4) If you try to print by "printf" any debug/Log information in the Console window, your program will crash every time in the first occurence of this operation: close all "printf".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a good day.&lt;/P&gt;&lt;P&gt;Evgeni&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 05 Apr 2013 05:59:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Target-not-run-after-flashing/m-p/249810#M9628</guid>
      <dc:creator>evgenik</dc:creator>
      <dc:date>2013-04-05T05:59:36Z</dc:date>
    </item>
  </channel>
</rss>