<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCU中的主题 Re: Error:  Initialization Failed.</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249355#M9580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the Project Wizard you can create an example for the processor and connection you're using.&lt;/P&gt;&lt;P&gt;this project will contain all default configuration needed.&lt;/P&gt;&lt;P&gt;You should be able to build it and debug the example application.&lt;/P&gt;&lt;P&gt;Is it working on your side ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jul 2013 14:11:42 GMT</pubDate>
    <dc:creator>trytohelp</dc:creator>
    <dc:date>2013-07-02T14:11:42Z</dc:date>
    <item>
      <title>Error:  Initialization Failed.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249354#M9579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="text-decoration: underline;"&gt;Code warrior development studio professional edition V 8.8&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;=== Target Configuration Settings&lt;/P&gt;&lt;P&gt;=== Connection:&amp;nbsp;&amp;nbsp; CodeWarrior USB TAP&lt;/P&gt;&lt;P&gt;=== Target Processor: 8349&lt;/P&gt;&lt;P&gt;Any idea to resolve this error?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 05:23:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249354#M9579</guid>
      <dc:creator>arunkumar_it</dc:creator>
      <dc:date>2013-07-02T05:23:47Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Initialization Failed.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249355#M9580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the Project Wizard you can create an example for the processor and connection you're using.&lt;/P&gt;&lt;P&gt;this project will contain all default configuration needed.&lt;/P&gt;&lt;P&gt;You should be able to build it and debug the example application.&lt;/P&gt;&lt;P&gt;Is it working on your side ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2013 14:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249355#M9580</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2013-07-02T14:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Initialization Failed.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249356#M9581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pascal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have created the project with the required configuration, when i try to program the processor with the&amp;nbsp; load, it shows&lt;/P&gt;&lt;P&gt;Initialization failed error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 04:06:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249356#M9581</guid>
      <dc:creator>arunkumar_it</dc:creator>
      <dc:date>2013-07-03T04:06:42Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Initialization Failed.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249357#M9582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It seems that the memory controller is not properly configured. Have you checked the memory operation with the help of the CodeWarrior Hardware Diagnostics applet?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 04:56:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249357#M9582</guid>
      <dc:creator>TICS_Fiona</dc:creator>
      <dc:date>2013-07-03T04:56:42Z</dc:date>
    </item>
    <item>
      <title>Re: Error:  Initialization Failed.</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249358#M9583</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Another point ...&lt;/P&gt;&lt;P&gt;There are seveal patches for CW for PA V8.8.&lt;/P&gt;&lt;P&gt;You can access them via the link:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-POWER-NETWORKING&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-POWER-NETWORKING&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;BR /&gt;expand the &lt;A class="inside_font" href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=CW-POWER-NETWORKING&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab"&gt;Updates and Patches (13)&lt;SPAN class="expand-all"&gt;&lt;STRONG&gt;Expand All&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/A&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The last path is PA V8.8.6 which require another patch V8.8.5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Pascal&lt;/P&gt;&lt;P align="right" class="filter-sort-area"&gt;&lt;SPAN class="sortModiifed"&gt;&lt;/SPAN&gt; &lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Jul 2013 06:23:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/Error-Initialization-Failed/m-p/249358#M9583</guid>
      <dc:creator>trytohelp</dc:creator>
      <dc:date>2013-07-03T06:23:44Z</dc:date>
    </item>
  </channel>
</rss>