<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: failed writing target address0 in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248970#M9568</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yeah, I wouldn't be surprised. I think I have to go back and revisit the custom BSP debugger files to make sure it is flashing correctly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 May 2013 15:47:00 GMT</pubDate>
    <dc:creator>FarhanH</dc:creator>
    <dc:date>2013-05-09T15:47:00Z</dc:date>
    <item>
      <title>failed writing target address0</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248967#M9565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp; Derek&lt;/P&gt;&lt;P&gt;We a brand new k20 PCB and are attempting to program with a P&amp;amp;E Multilink U. Programming the part failed with a "failed writing target address0" a hardware issue or a problem with the new BSP/PSP we set up.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119218i575A7EC3B233D7AE/image-size/large?v=v2&amp;amp;px=999" title="3743_3743.bmp" alt="3743_3743.bmp" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/39116i77E434C6074456CA/image-size/large?v=v2&amp;amp;px=999" title="ScreenShot108.bmp" alt="ScreenShot108.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Apr 2013 12:12:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248967#M9565</guid>
      <dc:creator>barbercolman</dc:creator>
      <dc:date>2013-04-02T12:12:08Z</dc:date>
    </item>
    <item>
      <title>Re: failed writing target address0</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248968#M9566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have the same exact issue with a K60 PCB and Multilink U. We have two custom boards that are duplicates and one of them has this issue. I am wondering whether it has something to do with the chip memory, as in, it has accidentally been locked.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 May 2013 23:21:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248968#M9566</guid>
      <dc:creator>FarhanH</dc:creator>
      <dc:date>2013-05-08T23:21:39Z</dc:date>
    </item>
    <item>
      <title>Re: failed writing target address0</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248969#M9567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Actually in this case I found that there was problems in how we built the BSP as well as issues in the debugger setup.&amp;nbsp; I do not remember the final solution, but the primary cause was operator error!.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 May 2013 15:43:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248969#M9567</guid>
      <dc:creator>barbercolman</dc:creator>
      <dc:date>2013-05-09T15:43:36Z</dc:date>
    </item>
    <item>
      <title>Re: failed writing target address0</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248970#M9568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yeah, I wouldn't be surprised. I think I have to go back and revisit the custom BSP debugger files to make sure it is flashing correctly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 May 2013 15:47:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/failed-writing-target-address0/m-p/248970#M9568</guid>
      <dc:creator>FarhanH</dc:creator>
      <dc:date>2013-05-09T15:47:00Z</dc:date>
    </item>
  </channel>
</rss>