<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 9S12DG256 Getting a Link Error: L1907 Fixup overflow in _FSFLOAT, to F_FRLONGK type 3, at of... in CodeWarrior for MCU</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129543#M955</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;You can fill up the remaining of the segment used for NON_BANKED later on with other content, just place the NON_BANKED mapping first.&lt;BR /&gt;&lt;BR /&gt;If INTERRUPT_ROUTINES is your own section which is compiled with -OnB=b, then you can place it to different segments.&lt;BR /&gt;As summary, if you place any section compiled with the near calling convention into multiple segments, then add the compiler option -OnB=b, the NON_BANKED thing is needed if you do not recompile rtshc12.c (or the whole ansi lib) with -OnB=b.&lt;BR /&gt;&lt;BR /&gt;rtshc12.c is located in lib\hc12c\src.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 06 Apr 2007 04:31:31 GMT</pubDate>
    <dc:creator>CompilerGuru</dc:creator>
    <dc:date>2007-04-06T04:31:31Z</dc:date>
    <item>
      <title>9S12DG256 Getting a Link Error: L1907 Fixup overflow in _FSFLOAT, to F_FRLONGK type 3, at offset 0x8</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129539#M951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;DIV&gt;9S12DG256 Getting a Link Error: L1907 Fixup overflow in _FSFLOAT, to F_FRLONGK type 3, at offset 0x8&amp;nbsp; linker fault.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;My code was compling and working, then I added a new group of 4 functions. When I enable all of them during compile/linking I get this fault.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What is this fault?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;P&gt;Message Edited by darrin on &lt;SPAN class="date_text"&gt;2007-04-04&lt;/SPAN&gt;&lt;SPAN class="time_text"&gt;08:52 PM&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2007 02:46:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129539#M951</guid>
      <dc:creator>darrin</dc:creator>
      <dc:date>2007-04-05T02:46:15Z</dc:date>
    </item>
    <item>
      <title>Re: 9S12DG256 Getting a Link Error: L1907 Fixup overflow in _FSFLOAT, to F_FRLONGK type 3, at of...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129540#M952</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;I asked google and found an answer I wrote some time ago, I guess you have the same issue as the OP of that thread. Daniel&lt;PRE&gt;The problem is that _LDIVS is calling NEG_P with a 8 bit relative offset:1233: void NEAR _LDIVS (void) { /* a = a / b signed */...000a 0700 BSR _NEG_P.. This works fine as long as you do allocate the NON_BANKED section into one single placement.However for your app it looks like all the others would just fill up the FLASH_PAGE4000 segment sothat _NEG_P does still fit into it and _LDIVS is allocated in FLASH_PAGEC000.So now what you can do about it:1. Change the allocation order in your prm file.The problem with this solution is that it does not really resolve the problem but instead it just tries to avoid it.2. Build rtshc12.c with the option -OnB=b.Either rebuild the whole library (lib\hc12c\hc12_lib.mcp) or add rtshc12.c to your project andadd the option in your project. For the second one, make sure rtshc12.c.o is before the ansi library in your link order.3. Distribute the NON_BANKED section manually to either FLASH_PAGE4000 or FLASH_PAGEC000, but not to both.&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2007 05:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129540#M952</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2007-04-05T05:50:29Z</dc:date>
    </item>
    <item>
      <title>Re: 9S12DG256 Getting a Link Error: L1907 Fixup overflow in _FSFLOAT, to F_FRLONGK type 3, at of...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129541#M953</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;I put NON_BANKED and INTERRUPT_ROUTINES into just 1 page and that appears to work.&lt;/DIV&gt;&lt;DIV&gt;I just hope I dont run out of room.&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;What is, and where can I get the file &amp;nbsp;rtshc12.c ?&lt;/DIV&gt;&lt;DIV&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV&gt;Thanks&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Apr 2007 20:54:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129541#M953</guid>
      <dc:creator>darrin</dc:creator>
      <dc:date>2007-04-05T20:54:40Z</dc:date>
    </item>
    <item>
      <title>Re: 9S12DG256 Getting a Link Error: L1907 Fixup overflow in _FSFLOAT, to F_FRLONGK type 3, at of...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129542#M954</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;You can fill up the remaining of the segment used for NON_BANKED later on with other content, just place the NON_BANKED mapping first. If INTERRUPT_ROUTINES is your own section which is compiled with -OnB=b, then you can place it to different segments. As summary, if you place any section compiled with the near calling convention into multiple segments, then add the compiler option -OnB=b, the NON_BANKED thing is needed if you do not recompile rtshc12.c (or the whole ansi lib) with -OnB=b. rtshc12.c is located in lib\hc12c\src. Daniel&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2007 04:31:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129542#M954</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2007-04-06T04:31:00Z</dc:date>
    </item>
    <item>
      <title>Re: 9S12DG256 Getting a Link Error: L1907 Fixup overflow in _FSFLOAT, to F_FRLONGK type 3, at of...</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129543#M955</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;You can fill up the remaining of the segment used for NON_BANKED later on with other content, just place the NON_BANKED mapping first.&lt;BR /&gt;&lt;BR /&gt;If INTERRUPT_ROUTINES is your own section which is compiled with -OnB=b, then you can place it to different segments.&lt;BR /&gt;As summary, if you place any section compiled with the near calling convention into multiple segments, then add the compiler option -OnB=b, the NON_BANKED thing is needed if you do not recompile rtshc12.c (or the whole ansi lib) with -OnB=b.&lt;BR /&gt;&lt;BR /&gt;rtshc12.c is located in lib\hc12c\src.&lt;BR /&gt;&lt;BR /&gt;Daniel&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Apr 2007 04:31:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/9S12DG256-Getting-a-Link-Error-L1907-Fixup-overflow-in-FSFLOAT/m-p/129543#M955</guid>
      <dc:creator>CompilerGuru</dc:creator>
      <dc:date>2007-04-06T04:31:31Z</dc:date>
    </item>
  </channel>
</rss>