<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックCodeWarrior v7.0 compiler executable</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243163#M9429</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was unable to configure Coverity Static Analysis v6.5.0 with the CodeWarrior v7.0 CmdIDE.exe compiler on Windows XP.&amp;nbsp; After talking with Coverity support, they explained that a non-IDE compiler executable needs to be used in order to do a build capture.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there or is there not a separate compiler executable that can be exercised on the command line, separate from the IDE, included in the CodeWarrior v7.0 installation?&amp;nbsp; If not, is there another version of CodeWarrior that does include a non-IDE compiler executable?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 30 Jan 2013 22:21:28 GMT</pubDate>
    <dc:creator>michaeld</dc:creator>
    <dc:date>2013-01-30T22:21:28Z</dc:date>
    <item>
      <title>CodeWarrior v7.0 compiler executable</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243163#M9429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was unable to configure Coverity Static Analysis v6.5.0 with the CodeWarrior v7.0 CmdIDE.exe compiler on Windows XP.&amp;nbsp; After talking with Coverity support, they explained that a non-IDE compiler executable needs to be used in order to do a build capture.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there or is there not a separate compiler executable that can be exercised on the command line, separate from the IDE, included in the CodeWarrior v7.0 installation?&amp;nbsp; If not, is there another version of CodeWarrior that does include a non-IDE compiler executable?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2013 22:21:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243163#M9429</guid>
      <dc:creator>michaeld</dc:creator>
      <dc:date>2013-01-30T22:21:28Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior v7.0 compiler executable</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243164#M9430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I assume you are targeting a ColdFire MCU.Am I right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Command line compiler is available in following location {Install}\ColdFire_Tools\Command_Line_Tools.&lt;/P&gt;&lt;P&gt;The compiler executable is called mwccmcf.exe, the assembler is called mwasmmcf.exe and the linker is called mwldmcf.exe.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to {Install}\Help\PDF\ColdFire_Build_Tools_Reference.pdf, chapter Using Build Tools on the Command Line for information of available options and required environment variables.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2013 07:33:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243164#M9430</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2013-01-31T07:33:07Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior v7.0 compiler executable</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243165#M9431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I am targeting a ColdFire MCU. I found the command line compiler where you specified.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now I am trying to use the compiler executable so that it identical to my IDE configuration.&amp;nbsp; The documentation you pointed too is helpful, but I already have the IDE configured and it would be nice to export the configuration options I already configured for the command line.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is unacceptable: &lt;A href="https://community.nxp.com/thread/36925"&gt;command-line options from Codewarrior IDE&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jan 2013 19:14:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243165#M9431</guid>
      <dc:creator>michaeld</dc:creator>
      <dc:date>2013-01-31T19:14:53Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior v7.0 compiler executable</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243166#M9432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not aware of any tools allowing to export IDE options settings into command line arguments.&lt;/P&gt;&lt;P&gt;CodeWarrior classic does not invoke the command line tools when building a project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The best location to retrieve the correspondence between IDE settings and command line arguments is the section &lt;EM&gt;&lt;STRONG&gt;IDE Settings Panels&lt;/STRONG&gt;&lt;/EM&gt; inside of the chapter using &lt;EM&gt;&lt;STRONG&gt;Build Tools with CodeWarrior IDE&lt;/STRONG&gt;&lt;/EM&gt; in the document I mentioned earlier.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CrasyCat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Feb 2013 06:51:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/CodeWarrior-v7-0-compiler-executable/m-p/243166#M9432</guid>
      <dc:creator>CrasyCat</dc:creator>
      <dc:date>2013-02-01T06:51:28Z</dc:date>
    </item>
  </channel>
</rss>