<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>CodeWarrior for MCUのトピックRe: create/add some sub-folders in my source folder</title>
    <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/create-add-some-sub-folders-in-my-source-folder/m-p/242266#M9398</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the simple way is to drag the folder from windows explore to the project folder in "CodeWarrior Projects" window directly. when you perform drag, CW will pop up message as below. you select the second or third. the folder link will be added to the project.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="link folder to project.JPG.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42770i12A0BF5E40D44F04/image-size/large?v=v2&amp;amp;px=999" role="button" title="link folder to project.JPG.jpg" alt="link folder to project.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Feb 2014 03:06:35 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2014-02-19T03:06:35Z</dc:date>
    <item>
      <title>create/add some sub-folders in my source folder</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/create-add-some-sub-folders-in-my-source-folder/m-p/242265#M9397</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Community,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;How can I create/add some sub-folders in the Source Folder once I create a new MQX project? &lt;/P&gt;&lt;P&gt;These sub-folders can contain some other source files which could be located in other locations rather than ‘source’ folder. &lt;/P&gt;&lt;P&gt;A good example would be web_hvac project in atheros_wifi package. As you can see in the figure in Source folder&lt;/P&gt;&lt;P&gt;there are some other folders like ‘enet’ or ‘phy’. The actual location of these folders are somewhere else rather than&lt;/P&gt;&lt;P&gt;in the ‘source’ folder in the hard drive; but they linked and showed up in source branch.&lt;/P&gt;&lt;P&gt;I use CW 10.5.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="9773_9773.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119720i7A21C8E91E427445/image-size/large?v=v2&amp;amp;px=999" role="button" title="9773_9773.jpg" alt="9773_9773.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="multi-folder.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42696i30B811C32BE22AED/image-size/large?v=v2&amp;amp;px=999" role="button" title="multi-folder.jpg" alt="multi-folder.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Feb 2014 17:12:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/create-add-some-sub-folders-in-my-source-folder/m-p/242265#M9397</guid>
      <dc:creator>amleng</dc:creator>
      <dc:date>2014-02-18T17:12:07Z</dc:date>
    </item>
    <item>
      <title>Re: create/add some sub-folders in my source folder</title>
      <link>https://community.nxp.com/t5/CodeWarrior-for-MCU/create-add-some-sub-folders-in-my-source-folder/m-p/242266#M9398</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;the simple way is to drag the folder from windows explore to the project folder in "CodeWarrior Projects" window directly. when you perform drag, CW will pop up message as below. you select the second or third. the folder link will be added to the project.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="link folder to project.JPG.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/42770i12A0BF5E40D44F04/image-size/large?v=v2&amp;amp;px=999" role="button" title="link folder to project.JPG.jpg" alt="link folder to project.JPG.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can this help?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2014 03:06:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/CodeWarrior-for-MCU/create-add-some-sub-folders-in-my-source-folder/m-p/242266#M9398</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2014-02-19T03:06:35Z</dc:date>
    </item>
  </channel>
</rss>